- Mon Jun 23, 2008 6:32 pm
#50728
I only came across this site recently, and it's like Christmas - all those electronics! Wow!
So I want to get back into playing with uCs, and I really like the USB Weather Board. But I want to make some changes, like add data logging in addition to BT, and a few other things.
My main concern is being able to change the program on the chip without the need for a programmer. I don't have a computer with a serial port, and I would prefer not to have to shell out for a programmer in any case. So I'm wondering if it would be possible to flash the Arduino boot loader onto the chip by using the existing UART pins, and perhaps manually pulling some pins to GND or whatever. Is that possible? It doesn't matter if it's a hack, I'll only need to do that once (hopefully) and then I'll just treat it like an Arduino.
Has anybody tried that? Any reasons why it should/should not work?
So I want to get back into playing with uCs, and I really like the USB Weather Board. But I want to make some changes, like add data logging in addition to BT, and a few other things.
My main concern is being able to change the program on the chip without the need for a programmer. I don't have a computer with a serial port, and I would prefer not to have to shell out for a programmer in any case. So I'm wondering if it would be possible to flash the Arduino boot loader onto the chip by using the existing UART pins, and perhaps manually pulling some pins to GND or whatever. Is that possible? It doesn't matter if it's a hack, I'll only need to do that once (hopefully) and then I'll just treat it like an Arduino.
Has anybody tried that? Any reasons why it should/should not work?