- Fri Apr 25, 2008 9:15 am
#47040
I'm looking at GPS modules to make a data aquisition system for a vehicle on a track and came across the EB-85A module. Seems to have pretty good accuracy, what I'm doing needs to have it be pretty accurate. I've read some similar products and they mention that their GPS modules have a 3m accuracy, but on a track, where areas are wide open and a wide view of the sky, they claim 1m. I'm hoping this is true and this unit will show similar characteristics.
One thing I was concerned with though is this unit doesn't have an external antenna. Maybe the SF photos don't show it, but I'm guessing the antenna is built into the module rather than being plugged into it? I'm concerned about the accuracy with it being mounted inside the car. I'm thinking it'll be on the dash, so it will have visibility through a windshield, but i'd really like to have an external antenna and mount it on the roof of the vehicle for the best possible locks.
I'm assuming the SirfIII units won't get the accuracy I'm looking for? I see the EM-408 has a connector for external antenna, but even with WAAS it says it only gets 5m.
I was also looking at some of the ublox modules, but there isn't as much data on people using them as there is with the units here. can anyone offer any advice that have used any of these modules? I've never done gps before, just trying to hopefully get it right the first time without wasting money.
One thing I was concerned with though is this unit doesn't have an external antenna. Maybe the SF photos don't show it, but I'm guessing the antenna is built into the module rather than being plugged into it? I'm concerned about the accuracy with it being mounted inside the car. I'm thinking it'll be on the dash, so it will have visibility through a windshield, but i'd really like to have an external antenna and mount it on the roof of the vehicle for the best possible locks.
I'm assuming the SirfIII units won't get the accuracy I'm looking for? I see the EM-408 has a connector for external antenna, but even with WAAS it says it only gets 5m.
I was also looking at some of the ublox modules, but there isn't as much data on people using them as there is with the units here. can anyone offer any advice that have used any of these modules? I've never done gps before, just trying to hopefully get it right the first time without wasting money.