- Mon Mar 31, 2008 8:30 am
#45582
I've bought a GM862-GPS module and breakout board. Everything worked all right in the beginning.
I used Hyperterminal to connect to the serial port. All AT commands returned OK. After inserting a SIM card I could place a data call by using ATD. I was also able to upload a python script using AT#WSCRIPT.
After a while the serial port did not respond anymore. The output became completely unreadable. I already tried different baud settings in Hyperterminal. However, when I connect the RS232 RX-line to the module TX_GPS Pin 35 and change baud rate to 4800, then I receive NMEA sentences perfectly readable.
What is going wrong? Why cannot I connect to the serial port anymore?
The module is powered through a 3,7 V Li-Po battery. The module TX- and RX-lines are connected to a MAX232. Between the GM862 TX-line and the MAX232 is a 4,7k ohm / 6,8k ohm resistor voltage divider in order to bring the 5V down to 3V, which is within the operating range for 2,8V CMOS. The MAX232 is connected to the RS232/DB9 port on the PC.
The Status LED flashes fast after turning the module on. When the SIM card is inserted, then after some seconds the LED is flashing slow. But the serial port output is always unreadable, regardless if the SIM card is inserted or not.
<EDIT>
Just when I power on the module, then I can type AT commands in Hyperterminal and receive OK. But a few seconds later the output becomes unreadable. When I turn the module off and then on again, the same thing. The module responds OK only for a few seconds.
</EDIT>
I used Hyperterminal to connect to the serial port. All AT commands returned OK. After inserting a SIM card I could place a data call by using ATD. I was also able to upload a python script using AT#WSCRIPT.
After a while the serial port did not respond anymore. The output became completely unreadable. I already tried different baud settings in Hyperterminal. However, when I connect the RS232 RX-line to the module TX_GPS Pin 35 and change baud rate to 4800, then I receive NMEA sentences perfectly readable.
What is going wrong? Why cannot I connect to the serial port anymore?
The module is powered through a 3,7 V Li-Po battery. The module TX- and RX-lines are connected to a MAX232. Between the GM862 TX-line and the MAX232 is a 4,7k ohm / 6,8k ohm resistor voltage divider in order to bring the 5V down to 3V, which is within the operating range for 2,8V CMOS. The MAX232 is connected to the RS232/DB9 port on the PC.
The Status LED flashes fast after turning the module on. When the SIM card is inserted, then after some seconds the LED is flashing slow. But the serial port output is always unreadable, regardless if the SIM card is inserted or not.
<EDIT>
Just when I power on the module, then I can type AT commands in Hyperterminal and receive OK. But a few seconds later the output becomes unreadable. When I turn the module off and then on again, the same thing. The module responds OK only for a few seconds.
</EDIT>