- Sun Feb 25, 2007 1:22 am
#26466
After many days of reading and trial and error to get the GM862 configured semi. I find myself needing to start to use python scripts which are VERY troublesome to get working correctly. You almost MUST have the ability to debug your scripts using one of the debugging methods available to the GM862. The problem is I have not found a solution that works with the SF board yet.
Has anyone got a working example of using debugging with this setup? Can you provide which FIRMWARE you are using and a step by step of how you got the process to work? I have tried both methods in the Easy Python Scripting PDF with no luck and have tried many variations in between.
The next step for me would be to try to use the EMMI TX port but from what I read it is dedicated to the NMEA stream of the GPS so I do not think it will work. Plus it has to be ran through a MAX232 in order to convert from the low voltage CMOS of the GM862 to a standard COM port voltage for a PC.
I hope someone has a better solution then this?
Has anyone got a working example of using debugging with this setup? Can you provide which FIRMWARE you are using and a step by step of how you got the process to work? I have tried both methods in the Easy Python Scripting PDF with no luck and have tried many variations in between.
The next step for me would be to try to use the EMMI TX port but from what I read it is dedicated to the NMEA stream of the GPS so I do not think it will work. Plus it has to be ran through a MAX232 in order to convert from the low voltage CMOS of the GM862 to a standard COM port voltage for a PC.
I hope someone has a better solution then this?