SparkFun Forums 

Where electronics enthusiasts find answers.

Discussions about carrier boards have here!
User avatar
By alembcke
#245338
I am trying to use the Sno M2 with the Input & Display carrier board. I can run GetXLR8Version just fine, as well as the Blink example. But when I try run the test sketch for the display I get nothing. I have made sure that I have all 3 of the required libraries installed and there are no errors when uploading the Example1_DisplayTest sketch to the Sno M2.

I noticed on the Input & Display Hookup Guide https://learn.sparkfun.com/tutorials/sp ... okup-guide that the Sno M2 is not shown under the "Required Materials" section. Does that mean it is not supported? Would it be possible to get the two working together, even if it is difficult?
#245339
Quick update, I just noticed this line at the top of the Input & Display Hookup Guide:
This nifty little board works with all SparkFun MicroMod processors...
I assume that includes the Sno M2, or does it not count as it is an FPGA and not a "processor?"
#245348
I quickly glanced at the schematics for the processor and carrier boards, and it looks like the screen should be accessible to the processor. It could be worth trying to find the pin definitions in the Arduino core library for the processor to check that they are all correct.

Have you tried accessing some of the other devices on the carrier board to check that they work with the example sketches?
#245357
I just tried the SparkFun MicroMod Button sketch, which reads whenever the buttons are pressed on the Input & Display carrier board. It worked perfectly, read every button press. So looks like the Sno M2 is communicating with the Input & Display carrier board just fine. It also looks like the screen works, the backlight is not, just blank.

My question really is if the HyperDisplay library is compatible with the Sno M2? If not, then I don't want to spin my wheels troubleshooting.
#245424
In the previous post I meant to say that the backlight is on, sorry for the typo.

Anyways, I tried the Adafruit ILI9341 library graphics test, as well as this MicroMod library https://github.com/paulvha/MicroMod/tree/main, and both do give me output showing that there is communication between the screen and the Sno M2:
Code: Select all
ILI9341 Test on MicroMod Input and Display carrier board!
Display Power Mode: 0xFF
MADCTL Mode: 0xFF
Pixel Format: 0xFF
Image Format: 0xFF
Self Diagnostic: 0xFF
Benchmark                Time (microseconds)
Screen fill              1303852
Text                     147332
Lines                    1199496
Horiz/Vert Lines         109820
Rectangles (outline)     72904
Rectangles (filled)      2707460
Circles (filled)         424272
Circles (outline)        511188
Triangles (outline)      265516
Triangles (filled)       1212032
Rounded rects (outline)  225924
Rounded rects (filled)   2735580
Done!
I also was able to get the LEDs to flash using the MicroMod library linked above. So at this point it looks like the screen is defective. I have contacted SparkFun to see what happens next.
#245462
So apparently the below being all 0xFF means that the SPI isn't working:
Code: Select all
Display Power Mode: 0xFF
MADCTL Mode: 0xFF
Pixel Format: 0xFF
Image Format: 0xFF
Self Diagnostic: 0xFF
Some boards you have to do some soldering - I hope that isn't the case with this board. I have been looking at the board schematics and trying any pin that looks like it might work. I get the above when I use the pins labeled DISP_CS, DISP_D/C and DISP_RST; which are 10, 18 and 44, respectively. Otherwise I get 0x0 for everything and the test hangs.
#245642
It might work, if the pinmap https://cdn.sparkfun.com/assets/learn_t ... OutMap.pdf (from here https://learn.sparkfun.com/tutorials/mi ... e-overview) can match the ones availed by the input board https://learn.sparkfun.com/tutorials/sp ... e-overview

Not all processors are suitable for all carrier boards, etc...let me know if the Sno doesn't end up suiting your use case
 Topic permissions

You can post new topics in this forum
You can reply to topics in this forum
You cannot edit your posts in this forum
You cannot delete your posts in this forum
You cannot post attachments in this forum