- Wed Jan 25, 2023 2:42 am
#238607
Hi
I've got the data logging board with the ESP32 processor board slotted in. I'm trying to use the SD card but am not having success. The example uses the Artemis processor and the schematic is fairly obvious as to what pins to use, however the ESP32 is not obvious. Can anyone point me in the right direction? I'm not sure if it is relevant but the errors I get are :-
On another note, why does is the upload so large compared to say the Artemis processor?
Bipman
I've got the data logging board with the ESP32 processor board slotted in. I'm trying to use the SD card but am not having success. The example uses the Artemis processor and the schematic is fairly obvious as to what pins to use, however the ESP32 is not obvious. Can anyone point me in the right direction? I'm not sure if it is relevant but the errors I get are :-
Code: Select all
I am also using the Expressif SD library too.E (29) gpio: GPIO can only be used as input mode
E (30) gpio: gpio_set_level(226): GPIO output gpio_num error
E (30) gpio: gpio_set_level(226): GPIO output gpio_num error
E (34) gpio: gpio_set_level(226): GPIO output gpio_num error
E (538) gpio: gpio_set_level(226): GPIO output gpio_num error
E (538) gpio: gpio_set_level(226): GPIO output gpio_num error
E (1038) gpio: gpio_set_level(226): GPIO output gpio_num error
On another note, why does is the upload so large compared to say the Artemis processor?
Bipman