- Mon Sep 21, 2020 9:10 am
#219104
I'm trying to get my Artemis Thing Plus to compile the DrawingBasics (in the HyperDisplay UG library) example for a Sparkfun Transparent OLED breakout. The example compiles for my Nano 33 so I believe this is an issue with the board. DrawingBasics had no issue with V 1.2.0 Apollo3, but did have an issue with BLE that was resolved in 2.0.1.
Artemis is using Apollo3 V. 2.0.1.
HyperDisplay Library V. 2.0.1
HyperDisplay_UG Library V. 1.1.0
HyperDisplay_SSD Library V. 1.1.1
Artemis is using Apollo3 V. 2.0.1.
HyperDisplay Library V. 2.0.1
HyperDisplay_UG Library V. 1.1.0
HyperDisplay_SSD Library V. 1.1.1
Code: Select all
Arduino: 1.8.13 (Windows 10), Board: "Artemis Thing Plus, 921600, Ambiq Secure Bootloader (Recommended)"
In file included from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src/HyperDisplay_SSD1309.h:19,
from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_Transparent_Graphical_OLED\src/HyperDisplay_UG2856KLBAG01.h:19,
from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\hudCodeMain\hudCodeMain.ino:3:
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay\src/hyperdisplay.h:25:2: warning: #warning "No custom configuration supplied for hyperdisplay, using default" [-Wcpp]
#warning "No custom configuration supplied for hyperdisplay, using default"
^~~~~~~
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\hudCodeMain\hudCodeMain.ino: In function 'void loop()':
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\hudCodeMain\hudCodeMain.ino:62:18: warning: unused variable 'warningWindowMem' [-Wunused-variable]
SSD1309_Bite_t warningWindowMem[20 * 20]; //allocate buffer memory
^~~~~~~~~~~~~~~~
In file included from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src/HyperDisplay_SSD1309.h:19,
from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_Transparent_Graphical_OLED\src\HyperDisplay_UG2856KLBAG01.h:19,
from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_Transparent_Graphical_OLED\src\HyperDisplay_UG2856KLBAG01.cpp:1:
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay\src/hyperdisplay.h:25:2: warning: #warning "No custom configuration supplied for hyperdisplay, using default" [-Wcpp]
#warning "No custom configuration supplied for hyperdisplay, using default"
^~~~~~~
In file included from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.h:19,
from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp:1:
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay\src/hyperdisplay.h:25:2: warning: #warning "No custom configuration supplied for hyperdisplay, using default" [-Wcpp]
#warning "No custom configuration supplied for hyperdisplay, using default"
^~~~~~~
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp: In member function 'virtual void SSD1309::swpixel(hd_extent_t, hd_extent_t, color_t, hd_colors_t, hd_colors_t)':
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp:249:17: warning: unused variable 'x0w' [-Wunused-variable]
hd_hw_extent_t x0w = (hd_hw_extent_t)x0; // Cast to hw extent type to be sure of integer values
^~~
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp:250:17: warning: unused variable 'y0w' [-Wunused-variable]
hd_hw_extent_t y0w = (hd_hw_extent_t)y0;
^~~
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp: In member function 'void SSD1309::lineClear(hd_extent_t, hd_extent_t, hd_extent_t, hd_extent_t, uint16_t)':
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp:346:18: warning: variable 'pix' set but not used [-Wunused-but-set-variable]
SSD1309_Bite_t pix;
^~~
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp: In member function 'virtual SSD1309_Status_t SSD1309_Arduino_I2C::writeBytes(uint8_t*, bool, size_t)':
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp:895:20: error: call of overloaded 'write(int)' is ambiguous
_i2c->write(0x00);
^
In file included from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.h:21,
from C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp:1:
C:\Users\dmjaf\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\2.0.1\libraries\Wire\src/Wire.h:39:20: note: candidate: 'virtual size_t arduino::MbedI2C::write(uint8_t)'
virtual size_t write(uint8_t data);
^~~~~
In file included from C:\Users\dmjaf\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\2.0.1/cores/arduino/mbed-bridge/core-api/api/Stream.h:25,
from C:\Users\dmjaf\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\2.0.1/cores/arduino/mbed-bridge/core-api/api/Client.h:22,
from C:\Users\dmjaf\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\2.0.1/cores/arduino/mbed-bridge/core-api/api/ArduinoAPI.h:29,
from C:\Users\dmjaf\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\2.0.1/cores/arduino/mbed-bridge/Arduino.h:14,
from C:\Users\dmjaf\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\2.0.1/cores/arduino/sdk/ArduinoSDK.h:9,
from <command-line>:
C:\Users\dmjaf\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\2.0.1/cores/arduino/mbed-bridge/core-api/api/Print.h:50:12: note: candidate: 'size_t arduino::Print::write(const char*)'
size_t write(const char *str) {
^~~~~
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp: In member function 'virtual SSD1309_Status_t SSD1309_Arduino_SPI::writeBytes(uint8_t*, bool, size_t)':
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp:935:10: warning: unused variable 'addr' [-Wunused-variable]
uint8_t addr = SSD1309_BASE_ADDR; // Not used in SPI mode but still set for good practice
^~~~
C:\Users\dmjaf\Desktop\HUD Project\Sparkfun Artemis Thing Plus\bluetoothSlave\libraries\SparkFun_HyperDisplay_SSD1309\src\HyperDisplay_SSD1309.cpp:937:19: warning: unused variable 'retval' [-Wunused-variable]
SSD1309_Status_t retval = SSD1309_Nominal;
^~~~~~
exit status 1
Error compiling for board Artemis Thing Plus.