- Wed Sep 16, 2020 4:07 pm
#219001
I like the Apollo3 in the Sparkfun Artemis module, but yowza, take a look at its new big brother the Apollo4:
Hey Sparkfun, any plans for an Artemis Module based on the Apollo4?
If the apollo4 clocking mechanisms are like the apollo3, it means that the apollo4 at 96 MHz will draw the same power as an apollo3 at 48 MHz. It would be amazing!
- 2M of MRAM (I think that means it is magnetoresistive non-volatile RAM instead of flash for program storage)
- 1.8M of SRAM
- Cortex M4 with floating point running at 96 MHz or 192 MHz processor clock
- USB interface
- Bluetooth LE
- MIPI Display Driver
- Crypto engine
- 3uA/MHz]
Hey Sparkfun, any plans for an Artemis Module based on the Apollo4?
If the apollo4 clocking mechanisms are like the apollo3, it means that the apollo4 at 96 MHz will draw the same power as an apollo3 at 48 MHz. It would be amazing!