- Wed Jul 29, 2020 11:21 pm
#217625
Hi there,
I am trying to reduce the power consumption of the Sparkfun Edge Board. (https://www.sparkfun.com/products/15170)
I found the previous post someone tried to do it. (viewtopic.php?p=217600#p217600)
"liquid.soulder" replied that always-powered sensors continuously drain power, so I desoldering 2 Mic sensors and BLE antenna.
I've tried examples from viewtopic.php?f=169&t=50904 and the below code
Deep Sleep @3V: 0.78mA
Sleep @3V: 0.88mA
Does anybody succeed to make Edge deep sleep?
Thx.
I am trying to reduce the power consumption of the Sparkfun Edge Board. (https://www.sparkfun.com/products/15170)
I found the previous post someone tried to do it. (viewtopic.php?p=217600#p217600)
"liquid.soulder" replied that always-powered sensors continuously drain power, so I desoldering 2 Mic sensors and BLE antenna.
I've tried examples from viewtopic.php?f=169&t=50904 and the below code
Code: Select all
But, these source codes do not work for the Sparkfun Edge . The measured current consumption (monosoon power monitor) are here:/*
Artemis Low Power: How low can we go?
By: Nathan Seidle
SparkFun Electronics
Date: October 17th, 2019
License: This code is public domain. Based on deepsleep.c from Ambiq SDK v2.2.0.
A big thanks to robin_hodgson for pointing out the HFRC shutdown requirement.
SparkFun labored with love to create this code. Feel like supporting open source hardware?
Buy a board from SparkFun! https://www.sparkfun.com/products/15376
How close can we get to 2.7uA in deep sleep?
This example shows how decrease the Artemis current consumption to less than ~2.5uA in deep sleep.
Note that Artemis modules with revision A1 silicon will use ~30uA. Please see the
Ambiq errata for more information: https://www.ambiqmicro.com/static/mcu/files/Apollo3_Blue_Errata_List_v1_0_external_release.pdf
To monitor the current to the Edge cut the MEAS jumper, solder in headers, and attach
a DMM via IC hooks (https://www.sparkfun.com/products/506).
The USB to serial bridge draws some current:
Serial Basic C - ~1.2uA (https://www.sparkfun.com/products/15096)
FTDI Basic - ~5.5uA (https://www.sparkfun.com/products/9873)
The various components on the Edge2 can be powered on/off as well
PDM microphones (2) - ~50.9uA
Accelerometer (POR mode) - ~79.7uA
Camera regulator enabled (no camera) - ~96.8uA
*/
void setup()
{
Serial.begin(115200);
Serial.println("Low power sleep example");
#if defined(ARDUINO_SFE_EDGE2)
pinMode(ACCEL_VDD, OUTPUT);
digitalWrite(ACCEL_VDD, LOW);
pinMode(MIC_VDD, OUTPUT);
digitalWrite(MIC_VDD, LOW);
pinMode(CAMERA_VDD, OUTPUT);
digitalWrite(CAMERA_VDD, LOW);
#endif
//Turn off ADC
power_adc_disable();
// Initialize for low power in the power control block
am_hal_pwrctrl_low_power_init();
// Stop the XTAL.
am_hal_clkgen_control(AM_HAL_CLKGEN_CONTROL_XTAL_STOP, 0);
// Disable the RTC.
am_hal_rtc_osc_disable();
// Disabling the debugger GPIOs saves about 1.2 uA total:
am_hal_gpio_pinconfig(20 /* SWDCLK */, g_AM_HAL_GPIO_DISABLE);
am_hal_gpio_pinconfig(21 /* SWDIO */, g_AM_HAL_GPIO_DISABLE);
// These two GPIOs are critical: the TX/RX connections between the Artemis module and the CH340S on the Blackboard
// are prone to backfeeding each other. To stop this from happening, we must reconfigure those pins as GPIOs
// and then disable them completely:
Serial.println("The TX and RX pins need to be disabled to minimize the current draw.");
Serial.println("You should not see any more Serial messages after this...");
delay(100);
am_hal_gpio_pinconfig(48 /* TXO-0 */, g_AM_HAL_GPIO_DISABLE);
am_hal_gpio_pinconfig(49 /* RXI-0 */, g_AM_HAL_GPIO_DISABLE);
// The default Arduino environment runs the System Timer (STIMER) off the 48 MHZ HFRC clock source.
// The HFRC appears to take over 60 uA when it is running, so this is a big source of extra
// current consumption in deep sleep.
// For systems that might want to use the STIMER to generate a periodic wakeup, it needs to be left running.
// However, it does not have to run at 48 MHz. If we reconfigure STIMER (system timer) to use the 32768 Hz
// XTAL clock source instead the measured deepsleep power drops by about 64 uA.
am_hal_stimer_config(AM_HAL_STIMER_CFG_CLEAR | AM_HAL_STIMER_CFG_FREEZE);
// This option selects 32768 Hz via crystal osc. This appears to cost about 0.1 uA versus selecting "no clock"
am_hal_stimer_config(AM_HAL_STIMER_XTAL_32KHZ);
// This option would be available to systems that don't care about passing time, but might be set
// to wake up on a GPIO transition interrupt.
// am_hal_stimer_config(AM_HAL_STIMER_NO_CLK);
// Turn OFF Flash1
if (am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_FLASH_512K))
{
while (1)
;
}
// Power down SRAM
PWRCTRL->MEMPWDINSLEEP_b.SRAMPWDSLP = PWRCTRL_MEMPWDINSLEEP_SRAMPWDSLP_ALLBUTLOWER32K;
Serial.println("Going to sleep...");
delay(100); //Wait for print to complete
Serial.end(); //Disable Serial
am_hal_sysctrl_sleep(AM_HAL_SYSCTRL_SLEEP_DEEP);
//We should never get here.
}
void loop()
{
//Do nothing
}
Deep Sleep @3V: 0.78mA
Sleep @3V: 0.88mA
Does anybody succeed to make Edge deep sleep?
Thx.