- Fri Jun 12, 2020 2:57 pm
#216198
I am currently using this Artemis RedBoard: https://www.sparkfun.com/products/15444.
I am also suing the following example from Ambiq SDK 2.2.0:
AmbiqSuite-Rel2.2.0\boards\apollo3_evb\examples\ble_freertos_amdtpc\gcc
I have added the following target to the provided Makefile for that example:
boot_artemis: wired_update
python3 ../../../../../tools/apollo3_scripts/ambiq_bin2board.py --bin $(CONFIG)/$(TARGET).bin \
--load-address-blob 0x20000 --magic-num 0xCB -o ${TARGET} \
--version 0x0 --load-address-wired 0x0C000 -i 6 --options 0x1 \
-b 115200 -port ${SERIAL_PORT} -r 2 -v
I can build and upload the code to the Artemis RedBoard using the git bash and above target with no error as seen below:
$ make boot_artemis
../../../../../tools/apollo3_scripts/create_cust_image_blob.py --bin bin/ble_freertos_amdtpc.bin --load-address 0x10000 --magic-num 0xCB -o bin/main_nonsecure_ota --version 0x0
Header Size = 0x80
original app_size 0x1d0bc ( 118972 )
load_address 0x10000 ( 65536 )
app_size 0x1d0bc ( 118972 )
w0 = 0xcb01d13c
Security Value 0x10
w2 = 0x10008080
addrWord = 0x10000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0xb97539d4
Writing to file bin/main_nonsecure_ota.bin
../../../../../tools/apollo3_scripts/create_cust_wireupdate_blob.py --load-address 0x20000 --bin bin/main_nonsecure_ota.bin -i 6 -o bin/main_nonsecure_wire --options 0x1
Header Size = 0x60
app_size 0x1d13c ( 119100 )
Writing to file bin/main_nonsecure_wire.bin
Image from 0x0 to 0x1d13c will be loaded at 0x20000
python3 ../../../../../tools/apollo3_scripts/ambiq_bin2board.py --bin bin/ble_freertos_amdtpc.bin \
--load-address-blob 0x20000 --magic-num 0xCB -o ble_freertos_amdtpc \
--version 0x0 --load-address-wired 0x10000 -i 6 --options 0x1 \
-b 115200 -port COM4 -r 2 -v
Header Size = 0x80
original app_size 0x1d0bc ( 118972 )
load_address 0x10000 ( 65536 )
app_size 0x1d0bc ( 118972 )
w0 = 0xcb01d13c
Security Value 0x10
w2 = 0x10008080
addrWord = 0x10000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0xb97539d4
Writing to file ble_freertos_amdtpc_OTA_blob.bin
testing: ble_freertos_amdtpc_OTA_blob.bin
Header Size = 0x60
app_size 0x1d13c ( 119100 )
Writing to file ble_freertos_amdtpc_Wired_OTA_blob.bin
Image from 0x0 to 0x1d13c will be loaded at 0x20000
Connecting over serial port COM4...
Sending Hello.
Received response for Hello
Bootloader connected
Received Status
length = 0x58
version = 0x5
Max Storage = 0x4ffa0
Status = 0x2
State = 0x7
AMInfo =
0x1
0xff2da3ff
0x55fff
0x1
0x4cd00005
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
Sending OTA Descriptor = 0xfe000
Sending Update Command.
number of updates needed = 1
Sending block of size 0x1d19c from 0x0 to 0x1d19c
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 4676
Sending Reset Command.
Tries = 0
Upload complete!
However, uploaded example is not producing any output and I am not sure if it is running or not.
I have also tried the load address of 0x10000 instead of 0x0C000 with no effect.
This example runs fine on the Edge board but not on the Artemis RedBoard.
I am also suing the following example from Ambiq SDK 2.2.0:
AmbiqSuite-Rel2.2.0\boards\apollo3_evb\examples\ble_freertos_amdtpc\gcc
I have added the following target to the provided Makefile for that example:
boot_artemis: wired_update
python3 ../../../../../tools/apollo3_scripts/ambiq_bin2board.py --bin $(CONFIG)/$(TARGET).bin \
--load-address-blob 0x20000 --magic-num 0xCB -o ${TARGET} \
--version 0x0 --load-address-wired 0x0C000 -i 6 --options 0x1 \
-b 115200 -port ${SERIAL_PORT} -r 2 -v
I can build and upload the code to the Artemis RedBoard using the git bash and above target with no error as seen below:
$ make boot_artemis
../../../../../tools/apollo3_scripts/create_cust_image_blob.py --bin bin/ble_freertos_amdtpc.bin --load-address 0x10000 --magic-num 0xCB -o bin/main_nonsecure_ota --version 0x0
Header Size = 0x80
original app_size 0x1d0bc ( 118972 )
load_address 0x10000 ( 65536 )
app_size 0x1d0bc ( 118972 )
w0 = 0xcb01d13c
Security Value 0x10
w2 = 0x10008080
addrWord = 0x10000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0xb97539d4
Writing to file bin/main_nonsecure_ota.bin
../../../../../tools/apollo3_scripts/create_cust_wireupdate_blob.py --load-address 0x20000 --bin bin/main_nonsecure_ota.bin -i 6 -o bin/main_nonsecure_wire --options 0x1
Header Size = 0x60
app_size 0x1d13c ( 119100 )
Writing to file bin/main_nonsecure_wire.bin
Image from 0x0 to 0x1d13c will be loaded at 0x20000
python3 ../../../../../tools/apollo3_scripts/ambiq_bin2board.py --bin bin/ble_freertos_amdtpc.bin \
--load-address-blob 0x20000 --magic-num 0xCB -o ble_freertos_amdtpc \
--version 0x0 --load-address-wired 0x10000 -i 6 --options 0x1 \
-b 115200 -port COM4 -r 2 -v
Header Size = 0x80
original app_size 0x1d0bc ( 118972 )
load_address 0x10000 ( 65536 )
app_size 0x1d0bc ( 118972 )
w0 = 0xcb01d13c
Security Value 0x10
w2 = 0x10008080
addrWord = 0x10000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0xb97539d4
Writing to file ble_freertos_amdtpc_OTA_blob.bin
testing: ble_freertos_amdtpc_OTA_blob.bin
Header Size = 0x60
app_size 0x1d13c ( 119100 )
Writing to file ble_freertos_amdtpc_Wired_OTA_blob.bin
Image from 0x0 to 0x1d13c will be loaded at 0x20000
Connecting over serial port COM4...
Sending Hello.
Received response for Hello
Bootloader connected
Received Status
length = 0x58
version = 0x5
Max Storage = 0x4ffa0
Status = 0x2
State = 0x7
AMInfo =
0x1
0xff2da3ff
0x55fff
0x1
0x4cd00005
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
Sending OTA Descriptor = 0xfe000
Sending Update Command.
number of updates needed = 1
Sending block of size 0x1d19c from 0x0 to 0x1d19c
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 8180
Sending Data Packet of length 4676
Sending Reset Command.
Tries = 0
Upload complete!
However, uploaded example is not producing any output and I am not sure if it is running or not.
I have also tried the load address of 0x10000 instead of 0x0C000 with no effect.
This example runs fine on the Edge board but not on the Artemis RedBoard.