Here's a mod to the sketch that will do 2 Channels at high speed. A 2kHz signal will put 2 completes waves in the buffer and I measure a sample frequency of 552kS/s per channel. As expected half the frequency of a single channel.
Code: Select all//*****************************************************************************
//
//! @file adc_lpmode0_dma.c
//!
//! @brief This example takes samples with the ADC at high-speed using DMA.
//!
//! Purpose: This example shows the CTIMER-A3 triggering repeated samples of an external
//! input at 1.2Msps in LPMODE0. The example uses the CTIMER-A3 to trigger
//! ADC sampling. Each data point is 8 sample average and is transferred
//! from the ADC FIFO into an SRAM buffer using DMA.
// uses bit-masking to parse out the data
#include "am_bsp.h"
// ADC Sample buffer.
#define ADC_SAMPLE_BUF_SIZE (1024) //2channels at 512 samples. Ch1 and Ch2 alternate in the buffer
uint32_t g_ui32ADCSampleBuffer[ADC_SAMPLE_BUF_SIZE];
unsigned long useconds_refresh;
// ADC Device Handle. Already declared.
//static void *g_ADCHandle;
// ADC DMA complete flag.
volatile bool g_bADCDMAComplete;
// ADC DMA error flag.
volatile bool g_bADCDMAError;
// Define the ADC SE0 pin to be used. (A4)
const am_hal_gpio_pincfg_t g_AM_PIN_16_ADCSE0 =
{
.uFuncSel = AM_HAL_PIN_16_ADCSE0,
};
// Define the ADC SE3 pin to be used. (A5)
const am_hal_gpio_pincfg_t g_AM_PIN_31_ADCSE3 =
{
.uFuncSel = AM_HAL_PIN_31_ADCSE3,
};
// Interrupt handler for the ADC.
//*****************************************************************************
extern "C" void am_adc_isr() //must use 'extern "C" ' for the Artemis
{
uint32_t ui32IntMask;
// Read the interrupt status.
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_status(g_ADCHandle, &ui32IntMask, false))
{
Serial.println("Error reading ADC interrupt status");
}
// Clear the ADC interrupt.
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_clear(g_ADCHandle, ui32IntMask))
{
Serial.println("Error clearing ADC interrupt status");
}
// If we got a DMA complete, set the flag.
if (ui32IntMask & AM_HAL_ADC_INT_DCMP)
{
g_bADCDMAComplete = true;
}
// If we got a DMA error, set the flag.
if (ui32IntMask & AM_HAL_ADC_INT_DERR)
{
g_bADCDMAError = true;
}
}
// Set up the core for sleeping, and then go to sleep.
//*****************************************************************************
void sleep()
{
// Disable things that can't run in sleep mode.
//#if (0 == ADC_EXAMPLE_DEBUG)
// am_bsp_debug_printf_disable();
//#endif
// Go to Deep Sleep.
am_hal_sysctrl_sleep(AM_HAL_SYSCTRL_SLEEP_DEEP);
// Re-enable peripherals for run mode.
//#if (0 == ADC_EXAMPLE_DEBUG)
// am_bsp_debug_printf_enable();
//#endif
}
// Configure the ADC.
//*****************************************************************************
void adc_config_dma()
{
am_hal_adc_dma_config_t ADCDMAConfig;
// Configure the ADC to use DMA for the sample transfer.
ADCDMAConfig.bDynamicPriority = true;
ADCDMAConfig.ePriority = AM_HAL_ADC_PRIOR_SERVICE_IMMED;
ADCDMAConfig.bDMAEnable = true;
ADCDMAConfig.ui32SampleCount = ADC_SAMPLE_BUF_SIZE;
ADCDMAConfig.ui32TargetAddress = (uint32_t)g_ui32ADCSampleBuffer;
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_dma(g_ADCHandle, &ADCDMAConfig))
{
Serial.println("Error - configuring ADC DMA failed.");
}
// Reset the ADC DMA flags.
g_bADCDMAComplete = false;
g_bADCDMAError = false;
}
// Configure the ADC.
//*****************************************************************************
void adc_config()
{
am_hal_adc_config_t ADCConfig;
am_hal_adc_slot_config_t ADCSlotConfig;
// Initialize the ADC and get the handle.
if ( AM_HAL_STATUS_SUCCESS != am_hal_adc_initialize(0, &g_ADCHandle) )
{
Serial.println("Error - reservation of the ADC instance failed.");
}
// Power on the ADC.
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_power_control(g_ADCHandle,
AM_HAL_SYSCTRL_WAKE,
false) )
{
//am_util_stdio_printf("Error - ADC power on failed.\n");
Serial.println("Error - ADC power on failed.");
}
// Set up the ADC configuration parameters. These settings are reasonable
// for accurate measurements at a low sample rate.
ADCConfig.eClock = AM_HAL_ADC_CLKSEL_HFRC;
ADCConfig.ePolarity = AM_HAL_ADC_TRIGPOL_RISING;
ADCConfig.eTrigger = AM_HAL_ADC_TRIGSEL_SOFTWARE;
ADCConfig.eReference = AM_HAL_ADC_REFSEL_INT_2P0;
/*
AM_HAL_ADC_REFSEL_INT_2P0,
AM_HAL_ADC_REFSEL_INT_1P5,
AM_HAL_ADC_REFSEL_EXT_2P0,
AM_HAL_ADC_REFSEL_EXT_1P5
*/
ADCConfig.eClockMode = AM_HAL_ADC_CLKMODE_LOW_LATENCY;
ADCConfig.ePowerMode = AM_HAL_ADC_LPMODE0;
ADCConfig.eRepeat = AM_HAL_ADC_REPEATING_SCAN; //AM_HAL_ADC_SINGLE_SCAN
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure(g_ADCHandle, &ADCConfig))
{
//am_util_stdio_printf("Error - configuring ADC failed.\n");
Serial.println("Error - configuring ADC failed.");
}
// Set up an ADC slot 0
ADCSlotConfig.eMeasToAvg = AM_HAL_ADC_SLOT_AVG_1;
ADCSlotConfig.ePrecisionMode = AM_HAL_ADC_SLOT_14BIT;
ADCSlotConfig.eChannel = AM_HAL_ADC_SLOT_CHSEL_SE0; //A4
ADCSlotConfig.bWindowCompare = false;
ADCSlotConfig.bEnabled = true;
/*
AM_HAL_ADC_SLOT_AVG_1,
AM_HAL_ADC_SLOT_AVG_2,
AM_HAL_ADC_SLOT_AVG_4,
AM_HAL_ADC_SLOT_AVG_8,
AM_HAL_ADC_SLOT_AVG_16,
AM_HAL_ADC_SLOT_AVG_32,
AM_HAL_ADC_SLOT_AVG_64,
AM_HAL_ADC_SLOT_AVG_128
AM_HAL_ADC_SLOT_14BIT,
AM_HAL_ADC_SLOT_12BIT,
AM_HAL_ADC_SLOT_10BIT,
AM_HAL_ADC_SLOT_8BIT
// Single-ended channels
AM_HAL_ADC_SLOT_CHSEL_SE0, (pad 16, ArtemisRB A4)
AM_HAL_ADC_SLOT_CHSEL_SE1, (pad 29, ArtemisRB A0)
AM_HAL_ADC_SLOT_CHSEL_SE2, (pad 11, ArtemisRB A1)
AM_HAL_ADC_SLOT_CHSEL_SE3, (pad 31, ArtemisRB A5)
AM_HAL_ADC_SLOT_CHSEL_SE4, (pad 32, ArtemisRB A8)
AM_HAL_ADC_SLOT_CHSEL_SE5, (pad 33, ArtemisRB A3)
AM_HAL_ADC_SLOT_CHSEL_SE6, (pad 34, ArtemisRB A2)
AM_HAL_ADC_SLOT_CHSEL_SE7, (pad 35, ArtemisRB n/a)
AM_HAL_ADC_SLOT_CHSEL_SE8, (pad 13, ArtemisRB A10)
AM_HAL_ADC_SLOT_CHSEL_SE9, (pad 12, ArtemisRB A9)
// Differential channels.
AM_HAL_ADC_SLOT_CHSEL_DF0, pads 12 (-), pad 13(+)
AM_HAL_ADC_SLOT_CHSEL_DF1, pads 15 (-), pad 14(+) (ArtemisRB n/a)
// Miscellaneous other signals.
AM_HAL_ADC_SLOT_CHSEL_TEMP,
AM_HAL_ADC_SLOT_CHSEL_BATT,
AM_HAL_ADC_SLOT_CHSEL_VSS
*/
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_slot(g_ADCHandle, 0, &ADCSlotConfig))
{
//am_util_stdio_printf("Error - configuring ADC Slot 0 failed.\n");
Serial.println("Error - configuring ADC Slot 0 failed.");
}
// Set up an ADC slot 1
ADCSlotConfig.eMeasToAvg = AM_HAL_ADC_SLOT_AVG_1;
ADCSlotConfig.ePrecisionMode = AM_HAL_ADC_SLOT_14BIT;
ADCSlotConfig.eChannel = AM_HAL_ADC_SLOT_CHSEL_SE3; //A5
ADCSlotConfig.bWindowCompare = false;
ADCSlotConfig.bEnabled = true;
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_slot(g_ADCHandle, 1, &ADCSlotConfig))
{
Serial.println("Error - configuring ADC Slot 0 failed.");
}
// Configure the ADC to use DMA for the sample transfer.
adc_config_dma();
//
am_hal_adc_interrupt_enable(g_ADCHandle, AM_HAL_ADC_INT_DERR | AM_HAL_ADC_INT_DCMP );
// Enable the ADC.
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_enable(g_ADCHandle))
{
Serial.println("Error - enabling ADC failed.");
}
}
// Initialize the ADC repetitive sample timer A3.
//*****************************************************************************
void init_timerA3_for_ADC()
{
// Start a timer to trigger the ADC periodically
am_hal_ctimer_config_single(3, AM_HAL_CTIMER_TIMERA,
AM_HAL_CTIMER_HFRC_12MHZ |
AM_HAL_CTIMER_FN_REPEAT |
AM_HAL_CTIMER_INT_ENABLE);
am_hal_ctimer_int_enable(AM_HAL_CTIMER_INT_TIMERA3);
am_hal_ctimer_period_set(3, AM_HAL_CTIMER_TIMERA, 10, 5); //10 tick period, 5 ticks wide
// Enable the timer A3 to trigger the ADC directly
am_hal_ctimer_adc_trigger_enable();
// Start the timer.
am_hal_ctimer_start(3, AM_HAL_CTIMER_TIMERA);
}
void setup() {
Serial.begin(115200);
while (!Serial) {}
Serial.println("2 Channel Hi-speed ADC test");
// Set the clock frequency.
if (AM_HAL_STATUS_SUCCESS != am_hal_clkgen_control(AM_HAL_CLKGEN_CONTROL_SYSCLK_MAX, 0))
{
Serial.println("Error - configuring the system clock failed.");
}
// Set the default cache configuration and enable it.
if (AM_HAL_STATUS_SUCCESS != am_hal_cachectrl_config(&am_hal_cachectrl_defaults))
{
Serial.println("Error - configuring the system cache failed.");
}
if (AM_HAL_STATUS_SUCCESS != am_hal_cachectrl_enable())
{
Serial.println("Error - enabling the system cache failed.");
}
// Configure the board for low power operation.
am_bsp_low_power_init();
// Enable only the first 512KB bank of Flash (0). Disable Flash(1)
if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_FLASH_MIN))
{
Serial.println("Error - configuring the flash memory failed.");
}
// Enable the first 32K of TCM SRAM.
if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_SRAM_32K_DTCM))
{
Serial.println("Error - configuring the SRAM failed.");
}
// Start the ITM interface.
//am_bsp_itm_printf_enable();
// Start the CTIMER A3 for timer-based ADC measurements.
init_timerA3_for_ADC();
// Enable interrupts.
NVIC_EnableIRQ(ADC_IRQn);
am_hal_interrupt_master_enable();
// Set a pin to act as our ADC input
am_hal_gpio_pinconfig(16, g_AM_PIN_16_ADCSE0); //artemis pad 16 is A4
am_hal_gpio_pinconfig(31, g_AM_PIN_31_ADCSE3); //artemis pad 31 is A5
// Configure the ADC
adc_config();
// Trigger the ADC sampling for the first time manually.
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_sw_trigger(g_ADCHandle))
{
Serial.println("Error - triggering the ADC failed.");
}
// Print the banner.
am_util_stdio_terminal_clear();
Serial.println("ADC Example with 1.2Msps and LPMODE=0");
// Allow time for all printing to finish.
am_util_delay_ms(10);
}
void loop() {
// Go to Deep Sleep.
useconds_refresh = micros();
if (!g_bADCDMAComplete)
{
sleep();
}
// Check for DMA errors.
if (g_bADCDMAError)
{
//am_util_stdio_printf("DMA Error occured\n");
Serial.println("DMA Error occured");
while (1);
}
// Check if the ADC DMA completion interrupt occurred.
if (g_bADCDMAComplete)
{
bool toggle = 0;
for (int i = 0; i < ADC_SAMPLE_BUF_SIZE; i++) {
//14 bit is 0-16383 on a range of 0-2V
uint32_t result = g_ui32ADCSampleBuffer[i];
uint32_t mask = 0xFFFC0; // all ones for bits 6-19, other bits zeroed
//Shift result depending on resolution, averaging
result = result & mask; //get bits 6-19 data only
result = result >> (6); //remove the fractional values
// Serial.println(result);
if (!toggle){
Serial.print(result * (2.0 / 16383.0), 3);
Serial.print(",");
}
else{
Serial.println(result * (2.0 / 16383.0), 3);
}
toggle = !toggle;
}
while (1) {} // stop to view data
// Reset the DMA completion and error flags.
g_bADCDMAComplete = false;
// Re-configure the ADC DMA.
adc_config_dma();
// Clear the ADC interrupts.
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_clear(g_ADCHandle, 0xFFFFFFFF))
{
//am_util_stdio_printf("Error - clearing the ADC interrupts failed.\n");
Serial.println("Error - clearing the ADC interrupts failed.");
}
// Trigger the ADC sampling for the first time manually.
if (AM_HAL_STATUS_SUCCESS != am_hal_adc_sw_trigger(g_ADCHandle))
{
//am_util_stdio_printf("Error - triggering the ADC failed.\n");
Serial.println("Error - triggering the ADC failed.");
}
}
}