- Tue Oct 01, 2019 6:25 am
#208174
Hi, everyone, I've been trying to upload code to the Artemis, with no success. This is what I've tried so far:
When using the Makefile to load the sketch the infamous port-is-currently-open error appears:
Arduino IDE
Also, I find strange that the result varies depending on the method. I'll keep investigating.
In anyone could help, I'd be really grateful
Cheers,
David.
- 2 Blackboard Artemis Nano and 1 Blackboard Artemis Uno
- Tested in 3 computers with Ubuntu 18 and one computer with Windows 10
- Versions of Arduino 1.8.9 and 1.8.10
- Drivers for the CH340 have been updated; module ch34x loaded, and ch341 unloaded.
- Several USB-C cables, some of them known to be working with SSD disks.
- Board definitions for the Sparkfun boards installed and up to date
- Upload baudrate set to 115200 in the IDE and in the Makefile from https://github.com/sparkfun/SparkFun_Ap ... Suite_BSPs
- Permissions and groups are OK
Code: Select all
The last error lines mean "The selected port cleared startup blip does not exist or the board is not connected."[10896] Failed to execute script artemis_svl
Traceback (most recent call last):
Artemis SVL Bootloader
File "artemis_svl.py", line 393, in <module>
File "artemis_svl.py", line 331, in main
phase: setup
File "artemis_svl.py", line 176, in phase_setup
cleared startup blip
File "artemis_svl.py", line 132, in wait_for_packet
phase: bootload
IndexError: index out of range
have 7464 bytes to send in 4 frames
error receiving packet
{'len': 0, 'cmd': 0, 'data': 0, 'crc': 1, 'timeout': 1}
unknown error
sending frame #0, length: 0
Upload failed
phase: setup
cleared startup blip
el puerto seleccionado cleared startup blip
no existe o tu placa no esta conectada
When using the Makefile to load the sketch the infamous port-is-currently-open error appears:
Code: Select all
If using bootloader_asb, the errors are:Artemis SVL Bootloader
phase: setup
cleared startup blip
phase: bootload
have 13240 bytes to send in 7 frames
error receiving packet
{'len': 0, 'cmd': 0, 'data': 0, 'crc': 1, 'timeout': 1}
unknown error
sending frame #0, length: 0
Upload failed
phase: setup
cleared startup blip
/dev/ttyUSB0 is currently open. Please close any other terminal programs that may be using /dev/ttyUSB0 and try again.
Arduino IDE
Code: Select all
Makefile[18321] Failed to execute script ambiq_bin2board
Traceback (most recent call last):
File "ambiq_bin2board.py", line 24, in <module>
ModuleNotFoundError: No module named 'am_defines'
ModuleNotFoundError: No module named 'am_defines'
Code: Select all
I've tested everything I found in forums and webs for days, and anything seems to work.Makefile:126: warning: you have not defined SDKPATH so will continue assuming that the SDK root is at ../../../../..
Makefile:134: warning: you have not defined COMMONPATH so will continue assuming that the COMMON root is at ../../../../common
Makefile:142: warning: you have not defined BOARDPATH so will continue assuming that the BOARD root is at ../../..
Makefile:150: warning: you have not defined PROJECTPATH so will continue assuming that the PROJECT root is at ..
/usr/bin/python3 ../../../../common/tools_sfe/ambiq/ambiq_bin2board.py --bin bin/example_asb.bin --load-address-blob 0x20000 --magic-num 0xCB -o bin/example --version 0x0 --load-address-wired 0xC000 -i 6 --options 0x1 -b 115200 -port /dev/ttyUSB0 -r 2 -v
Header Size = 0x80
original app_size 0x33b8 ( 13240 )
load_address 0xc000 ( 49152 )
app_size 0x33b8 ( 13240 )
w0 = 0xcb003438
Security Value 0x10
w2 = 0x10008080
addrWord = 0xc000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0x944f7ce5
Writing to file bin/example_OTA_blob.bin
testing: bin/example_OTA_blob.bin
Header Size = 0x60
app_size 0x3438 ( 13368 )
Writing to file bin/example_Wired_OTA_blob.bin
Image from 0x0 to 0x3438 will be loaded at 0x20000
Connecting over serial port /dev/ttyUSB0...
Sending Hello.
Received response for Hello
Received Unknown Message
msgType = 0x0
Length = 0x0
['0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0']
Fail
Sending Hello.
Received response for Hello
Received Unknown Message
msgType = 0x0
Length = 0x0
['0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0']
Fail
Sending Hello.
Received response for Hello
Received Unknown Message
msgType = 0x0
Length = 0x0
['0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0']
Fail
Tries = 3
Upload failed
Also, I find strange that the result varies depending on the method. I'll keep investigating.
In anyone could help, I'd be really grateful
Cheers,
David.