SparkFun Forums 

Where electronics enthusiasts find answers.

Hardware or product specific questions are best asked here.
User avatar
By robin_hodgson
#208302
A JLink EDU ($60 from Sparkfun). My understanding is that the setup will also work with a JLink EDU Mini ($18 at Sparkfun), it will just be a bit slower than the more expensive one.
User avatar
By VA3SU
#208303
Much better than the ~$400-$900 dollar ones lol. BTW my Redboard draws 2.48-2.54uA and it doesn't change when on or off the bench held in hand etc. Warming it up with fingers brings it above 2.6uA breath about the same. Using a Rigol DM3058e no averaging.
User avatar
By robin_hodgson
#208329
Getting to the root of "6 uA per MHz":

Take a look at the clock diagram in the Apollo3 data sheet. If you zoom in on the part at the bottom showing where the CPU gets its clock (attached), you can see that the signal marked "hclk/fclk to CPU/SRAM/Cache" only has two possible frequencies that can be selected from the multiplexer: 48 MHz or 96 MHz. There are a total of three various divider blocks in the original diagram (only one of them is visible in the attachment), but none of the three has an output that goes to the processor/SRAM/cache. The upshot is that when the data sheet says "6 uA per MHz", there is an implicit multiplier of 48 because the slowest the processor can run is 48 MHz. So: the lowest typical current draw that a running program could have would be 6 uA/MHz *48 MHz, or 288 uA.

In regards to a comment way earlier in this thread about a processor "running at 3 MHz", it is clear that something inside the processor might have been getting clocked at 3 MHz, but it couldn't have been the processor itself.
You do not have the required permissions to view the files attached to this post.
User avatar
By robin_hodgson
#208338
All industry datasheets involve a certain amount of specmanship.

I did find something else this morning. It would appear that there is a master clock divider for HFRC where it can be divided by 2, if desired. See attached register description. The diagram of clock sources in the data sheet does not show an HFRC master divider, but if so, the processor would be capable of running at 96 MHz, 48 MHz, or 24 MHz. I'll try to verify that today.
You do not have the required permissions to view the files attached to this post.
User avatar
By robin_hodgson
#208339
Yup, it's confirmed that the core clock divisor works as described. Running a while (1); at 24 MHz drops the current to about 60% of the current at 48 MHz. As always, running at 24 MHz means that it will take twice as long to perform the same set of instructions than running at 48 MHz, so while the peak current consumption will be lower at 24 MHz, the energy consumed to perform an identical set of instructions is actually higher at 24 MHz than 48 MHz.
User avatar
By username_is_too_long
#218411
Hey robin_hodgson, i tried this clock division with a freertos program and it works. So nice, again thank you for the information!
-Turo
 Topic permissions

You can post new topics in this forum
You can reply to topics in this forum
You cannot edit your posts in this forum
You cannot delete your posts in this forum
You cannot post attachments in this forum