SparkFun Forums 

Where electronics enthusiasts find answers.

Questions &/or issues related to products in the Environment category should be posted in this forum. Includes Air Quality, Altitude, Atmospheric & barometric pressure, Combo boards & other, Temperature & humidity, etc.
User avatar
By TS-Mark
#205344
Hi valter92,

Since this is an analog accelerometer, the latency is going to be extremely low. Any significant delay in this would be created by the controller it is attached to. The tuning capacitors we populate on this board sets the bandwidth to 50Hz but you can theoretically get up to 1600Hz on the X and Y axes and 550Hz on the Z axis. For more information on that, I would recommend reading through the datasheet for the ADXL335.