SparkFun Forums 

Where electronics enthusiasts find answers.

Have questions about a SparkFun product or board? This is the place to be.
By Systembolaget
#201427
Hej,

I want to drive 34V 90mA, 180mA and 360mA COB LEDs with a FemtoBuck and a Li-Po battery and saw that the FemtoBuck needs 6V input minimum - a single cell 3.7V Li-Po battery won't be enough, so I need a 2S version with 7.4V for the input to be boosted to 34V.

Will that work?

Also, how could I reduce the constant current from the default 330mA down to 90 and 180mA?

Many thanks in advance!