- Wed Oct 03, 2018 3:20 pm
#200552
hello evryone!
i`m a bit confused with the next thing. So i have x and y coords. I need do do an IF expression when both conditions are performed. Condition for X is when its in a range from 0,00 to 100,00 or over 230,00 and at the same time Y is in the range from 0,00 to 20,00 or over 180 then do {}
i`ve made it like
if (x<=100 || x>=230 && (y>=180 || y<20))
{
}
But you know its not working lika a charm...
Maybe there is a better solution for such logic like using an array? Im a newbie so don kick me too much))) Thanks guys!
i`m a bit confused with the next thing. So i have x and y coords. I need do do an IF expression when both conditions are performed. Condition for X is when its in a range from 0,00 to 100,00 or over 230,00 and at the same time Y is in the range from 0,00 to 20,00 or over 180 then do {}
i`ve made it like
if (x<=100 || x>=230 && (y>=180 || y<20))
{
}
But you know its not working lika a charm...
Maybe there is a better solution for such logic like using an array? Im a newbie so don kick me too much))) Thanks guys!