- Tue Nov 14, 2017 1:00 am
#196955
Hi,
First of all, I'm sorry if I'm posting this thread in the wrong board. This is my first post so I'm not really experienced here. I hope to be soon!
I've been working on a Raspberry Pi project where I gather the readings of a CCS811 and a DHT11 sensor and then send them to a MySQL database for readout later.
I use a singular Python script containing the following functions:
Here is the Python script I use to do all of this. I hope someone can possibly point me in the right direction as to how I can fix this.
First of all, I'm sorry if I'm posting this thread in the wrong board. This is my first post so I'm not really experienced here. I hope to be soon!
I've been working on a Raspberry Pi project where I gather the readings of a CCS811 and a DHT11 sensor and then send them to a MySQL database for readout later.
I use a singular Python script containing the following functions:
- A 4 way DIP switch to generate a unique ID for the Raspberry Pi (Goal is to use multiple sensors in multiple rooms).
- A function to only send the data if there is internet connection, if there is no internet connection a LED will start blinking rapidly.
- Function where I read out values of CCS811 and DHT11 and send it via GET request to DB.
- Logging all data to a local textfile on the Raspberry PI.
- After receiving very volatile readings from the CCS811 I started using a Arduino to measure the voltage from the Raspberry pi, singling out the problems that could be causing the weird readings.
Here is the Python script I use to do all of this. I hope someone can possibly point me in the right direction as to how I can fix this.
Code: Select all
and also the library I use for the CCS811:
#!/usr/bin/python
# -*- coding: utf-8 -*-
# By Olivier van Heulen
# Student at Scalda College
# Working on Kelvin
# 206374@student.scalda.nl
import RPi.GPIO as GPIO
import dht11
import smbus
import time
import urllib3.request
from datetime import datetime
import socket
bus = smbus.SMBus(1)
adress = 0x04
GPIO.setmode(GPIO.BCM)
GPIO.setup(17, GPIO.OUT)
GPIO.setup(14, GPIO.IN, pull_up_down=GPIO.PUD_UP)
GPIO.setup(15, GPIO.IN, pull_up_down=GPIO.PUD_UP)
GPIO.setup(18, GPIO.IN, pull_up_down=GPIO.PUD_UP)
GPIO.setup(27, GPIO.IN, pull_up_down=GPIO.PUD_UP)
instance = dht11.DHT11(pin=0x04)
from CCS811_RPi import CCS811_RPi
ccs811 = CCS811_RPi()
http = urllib3.PoolManager()
url = 'removed for post'
# Do you want to preset sensor baseline? If yes set the value here, otherwise set False
INITIALBASELINE = False
# Set MEAS_MODE (measurement interval)
configuration = 0b100000
# Set read interval for retriveving last measurement data from the sensor
pause = 60
print 'Checking hardware ID...'
print ccs811.checkHWID()
hwid = ccs811.checkHWID()
print hwid
if hwid == hex(129):
print 'Hardware ID is correct'
else:
print ('Incorrect hardware ID ', hwid, ', should be 0x81')
def internet(host='8.8.8.8', port=53, timeout=3):
try:
socket.setdefaulttimeout(timeout)
socket.socket(socket.AF_INET,
socket.SOCK_STREAM).connect((host, port))
return True
except Exception, ex:
return False
# print 'MEAS_MODE:',ccs811.readMeasMode()
ccs811.configureSensor(configuration)
print ('MEAS_MODE:', ccs811.readMeasMode())
print ('STATUS: ', bin(ccs811.readStatus()))
print '---------------------------------'
# Use these lines if you need to pre-set and check sensor baseline value
if INITIALBASELINE > 0:
ccs811.setBaseline(INITIALBASELINE)
print ccs811.readBaseline()
print 'Waiting 60 seconds for sensor to initialize'
time.sleep(60)
print '---------------------------------'
if internet() == True:
while 1:
x = 0
if GPIO.input(14) == 1:
x = x + 1
if GPIO.input(15) == 1:
x = x + 2
if GPIO.input(18) == 1:
x = x + 0x04
if GPIO.input(27) == 1:
x = x + 8
statusbyte = ccs811.readStatus()
print ('STATUS: ', bin(statusbyte))
print ('Raspberry ID according to DIP: ', x)
error = ccs811.checkError(statusbyte)
if error:
print ('ERROR:', ccs811.checkError(statusbyte))
if not ccs811.checkDataReady(statusbyte):
GPIO.output(17, 1)
print 'No new samples are ready'
print '---------------------------------'
time.sleep(0.1)
GPIO.output(17, 0)
time.sleep(0.1)
GPIO.output(17, 1)
time.sleep(0.1)
GPIO.output(17, 0)
time.sleep(pause)
continue
result1 = instance.read()
print (result1.temperature)
print (result1.humidity)
if result1.temperature > 0:
if result1.humidity > 0:
print("dht gave reading, compensating.")
ccs811.setCompensation(result1.temperature, result1.humidity)
else:
print("dht didnt give reading, no compensation this time.")
continue;
result = ccs811.readAlg()
if not result:
print 'Invalid result received'
time.sleep(pause)
continue
GPIO.output(17, 1)
baseline = ccs811.readBaseline()
print ('eCO2: ', result['eCO2'], ' ppm')
print ('TVOC: ', result['TVOC'], 'ppb')
# print 'Status register: ',bin(result['status'])
print ('Last error ID: ', result['errorid'])
# print 'RAW data: ',result['raw']
# print 'Baseline: ',baseline
ppm = result['eCO2']
with open('/home/pi/logoffline.txt', 'a') as logger:
byte_data = bus.read_i2c_block_data(adress, 2)
voltage = float((byte_data[0] << 8) + byte_data[1])
print byte_data[0]
print byte_data[1]
print 2 * (5 * voltage / 1023)
logger.write(str(datetime.now().strftime('%Y-%m-%d %H:%M:%S'
) + ' eCO2: ' + str(result['eCO2']) + ' TVOC: '
+ str(result['TVOC']) + ' error ID: '
+ str(result['errorid']) + ' Voltage: '
+ str(2 * (5 * voltage / 1023)) + '\n'))
logger.close
if result1.is_valid():
temperature = result1.temperature
humidity = result1.humidity
try:
# r=http.request('GET',url,fields={'id':x, 'temp':temperature,'hum' :humidity,'co2':ppm})
print r.data.decode('utf-8')
print '---------------------------------'
except:
print 'Error connecting to server, skiping this reading'
continue
print '---------------------------------'
time.sleep(0.5)
GPIO.output(17, 0)
time.sleep(pause)
if internet() == False:
print 'no internet'
while internet() == False:
GPIO.output(17, 1)
time.sleep(0.1)
GPIO.output(17, 0)
time.sleep(0.1)
print 'still no internett'
Code: Select all
TL;DR: I am using a CCS811 sensor to read Co2 sensors but the readings I am getting are not making any sense whatsoever. I am not sure what I'm doing wrong.#
# CCS811_RPi
#
# Petr Lukas
# July, 11 2017
#
# Version 1.0
import struct, array, time, io, fcntl
# I2C Address
CCS811_ADDRESS = (0x5B)
# Registers
CCS811_HW_ID = (0x20)
CSS811_STATUS = (0x00)
CSS811_APP_START = (0xF4)
CSS811_MEAS_MODE = (0x01)
CSS811_ERROR_ID = (0xE0)
CSS811_RAW_DATA = (0x03)
CSS811_ALG_RESULT_DATA = (0x02)
CSS811_BASELINE = (0x11)
CSS811_ENV_DATA = (0x05)
# Errors ID
ERROR = {}
ERROR[0] = 'WRITE_REG_INVALID'
ERROR[1] = 'READ_REG_INVALID'
ERROR[2] = 'MEASMODE_INVALID'
ERROR[3] = 'MAX_RESISTANCE'
ERROR[4] = 'HEATER_FAULT'
ERROR[5] = 'HEATER_SUPPLY'
I2C_SLAVE = 0x0703
CCS811_fw = 0
CCS811_fr = 0
class CCS811_RPi:
def __init__(self, twi=1, addr=CCS811_ADDRESS):
global CCS811_fr, CCS811_fw
CCS811_fr = io.open("/dev/i2c-" + str(twi), "rb", buffering=0)
CCS811_fw = io.open("/dev/i2c-" + str(twi), "wb", buffering=0)
# set device address
fcntl.ioctl(CCS811_fr, I2C_SLAVE, CCS811_ADDRESS)
fcntl.ioctl(CCS811_fw, I2C_SLAVE, CCS811_ADDRESS)
time.sleep(0.015)
# public functions
def checkHWID(self):
s = [CCS811_HW_ID] # Hardware ID
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.0625)
data = CCS811_fr.read(1)
buf = array.array('B', data)
return hex(buf[0])
def readStatus(self):
time.sleep(0.015)
s = [CSS811_STATUS]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.0625)
data = CCS811_fr.read(1)
buf = array.array('B', data)
return buf[0]
def checkError(self, status_byte):
time.sleep(0.015)
error_bit = ((status_byte) >> 0) & 1
if (not error_bit):
return False
s = [CSS811_ERROR_ID]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.0625)
data = CCS811_fr.read(1)
buf = array.array('B', data)
return ERROR[int(buf[0])]
def configureSensor(self, configuration):
# Switch sensor to application mode
s = [CSS811_APP_START]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.0625)
s = [CSS811_MEAS_MODE, configuration, 0x00]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.015)
return
def readMeasMode(self):
time.sleep(0.015)
s = [CSS811_MEAS_MODE]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.0625)
data = CCS811_fr.read(1)
buf = array.array('B', data)
return bin(buf[0])
def readRaw(self):
time.sleep(0.015)
s = [CSS811_RAW_DATA]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.0625)
data = CCS811_fr.read(2)
buf = array.array('B', data)
return (buf[0] * 256 + buf[1])
def readAlg(self):
time.sleep(0.015)
s = [CSS811_ALG_RESULT_DATA]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.0625)
data = CCS811_fr.read(8)
buf = array.array('B', data)
result = {}
# Read eCO2 value and check if it is valid
result['eCO2'] = buf[0] * 256 + buf[1]
if (result['eCO2'] > 8192):
print('Invalid eCO2 value')
return False
# Read TVOC value and check if it is valid
result['TVOC'] = buf[2] * 256 + buf[3]
if (result['TVOC'] > 1187):
print('Invalid TVOC value')
return False
result['status'] = buf[4]
# Read the last error ID and check if it is valid
result['errorid'] = buf[5]
if (result['errorid'] > 5):
print('Invalid Error ID')
return False
result['raw'] = buf[6] * 256 + buf[7]
return result
def readBaseline(self):
time.sleep(0.015)
s = [CSS811_BASELINE]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.0625)
data = CCS811_fr.read(2)
buf = array.array('B', data)
return (buf[0] * 256 + buf[1])
def checkDataReady(self, status_byte):
ready_bit = ((status_byte) >> 3) & 1
if (ready_bit):
return True
else:
return False
def setCompensation(self, temperature, humidity):
temperature = round(temperature, 2)
humidity = round(humidity, 2)
print('Setting compensation to ', temperature, ' C and ', humidity, ' %')
hum1 = int(humidity // 0.5)
hum2 = int(humidity * 512 - hum1 * 256)
temperature = temperature + 25
temp1 = int(temperature // 0.5)
temp2 = int(temperature * 512 - temp1 * 256)
s = [CSS811_ENV_DATA, hum1, hum2, temp1, temp2, 0x00]
s2 = bytearray(s)
CCS811_fw.write(s2)
return
def setBaseline(self, baseline):
print('Setting baseline to ', baseline)
buf = [0, 0]
s = struct.pack('>H', baseline)
buf[0], buf[1] = struct.unpack('>BB', s)
print(buf[0])
print(buf[1])
s = [CSS811_BASELINE, buf[0], buf[1], 0x00]
s2 = bytearray(s)
CCS811_fw.write(s2)
time.sleep(0.015)