SparkFun Forums 

Where electronics enthusiasts find answers.

General project discussion / help
Did you make a robotic coffee pot which implements HTCPCP and decafs unauthorized users? Show it off here!
#198596
Hi. Currently, I am working on getting the raspberry pi 2 to communicate with my iboard avr via a usb-to-serial-port adapter cable for the main purpose of controlling the dc motors already connected to the iboard avr(atmega16). I have already installed the packages for avrdude and enabled the python serial port on rpi 2.
After installing the avrdude libraries, As instructed, I tried both siprog and ponyser and got the following results:
avrdude -c ponyser -P /dev/ttyUSB0 -e -p m16 -U lfuse:w:0xff:m -U hfuse:w:0xc9:m -F
avrdude: AVR device initialized and ready to accept instructions
Reading | ################################################## | 100% 0.10s
avrdude: Device signature = 0x000000 (retrying)
Reading | ################################################## | 100% 0.09s
avrdude: Device signature = 0x000102
avrdude: Expected signature for ATmega16 is 1E 94 03
avrdude: erasing chip
avrdude: AVR device not responding
avrdude: reading input file "0xff"
avrdude: writing lfuse (1 bytes):
Writing | | 0% 0.00s ***failed;
Writing | ################################################## | 100% 0.23s
avrdude: 1 bytes of lfuse written
avrdude: verifying lfuse memory against 0xff:
avrdude: load data lfuse data from input file 0xff:
avrdude: input file 0xff contains 1 bytes
avrdude: reading on-chip lfuse data:
Reading | ################################################## | 100% 0.03s
avrdude: verifying …
avrdude: verification error, first mismatch at byte 0x0000
0x14 != 0xff
avrdude: verification error; content mismatch
avrdude: safemode: Verify error - unable to read lfuse properly. Programmer may not be reliable.
avrdude: safemode: Verify error - unable to read lfuse properly. Programmer may not be reliable.
avrdude: safemode: Sorry, reading back fuses was unreliable. I have given up and exited programming mode
avrdude done. Thank you.
avrdude -c siprog -P /dev/ttyUSB0 -e -p m16 -U lfuse:w:0xff:m -U hfuse:w:0xc9:m -F
avrdude: AVR device initialized and ready to accept instructions
Reading | ################################################## | 100% 0.08s
avrdude: Device signature = 0x1e9403
avrdude: safemode: Verify error - unable to read lfuse properly. Programmer may not be reliable.
avrdude: safemode: To protect your AVR the programming will be aborted
avrdude done. Thank you.
In both options , I had to include -F to override the signature check otherwise, I was getting this:
avrdude -c ponyser -P /dev/ttyUSB0 -e -p m16 -U lfuse:w:0xff:m -U hfuse:w:0xc9:m
avrdude: AVR device not responding
avrdude: initialization failed, rc=-1
Double check connections and try again, or use -F to override
this check.
Overall, the problem now seems to be with reading the lfuse for some reason. Any thoughts? Can't seem to upload the attached pdfs of the iboard kit I am using with rpi 2