- Thu Nov 09, 2017 4:31 pm
#196911
I am working on a project to add a police lightbar and other lights to a military humvee for my local Police Department to use in inclement weather. The humvee is 24V system with 2 large 12V batteries in series. Some of the equipment is 12V and some is 24V. To prevent draining the batteries I would like to install one master switch that will disable all of the added gear when in the open position and control two circuits, one 12V and one 24V. So, when in closed position the 12V and 24V equipment will have power to them.
What type of switch do I need to buy? I would prefer a toggle switch with a built in LED.
Harley
What type of switch do I need to buy? I would prefer a toggle switch with a built in LED.
Harley