- Mon Sep 11, 2017 9:33 pm
#196128
I use Altera USB-Blaster rev.C. So far I launch without target. When I try to send the "target remote localhost:3333" command to gdb I see that nobody answers gdb during the given timeout. Here a log the removed openocd:
What do I do not so?
Code: Select all
It seems to me that the initialization connected to the Altera USB-Blaster adapter does not come to the end also to a stage when gdb can set connection with openocd does not reach.user@debian:~$ sudo openocd -d -c "log_output openocd.log" -f altera-usb-blaster.cfg
[sudo] password for user:
Open On-Chip Debugger 0.10.0+dev-00172-g7719e96 (2017-09-11-13:32)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
User : 13 18 command.c:544 command_print(): debug_level: 3
Debug: 14 18 options.c:181 add_default_dirs(): bindir=/usr/local/bin
Debug: 15 18 options.c:182 add_default_dirs(): pkgdatadir=/usr/local/share/openocd
Debug: 16 18 options.c:183 add_default_dirs(): exepath=/usr/local/bin
Debug: 17 18 options.c:184 add_default_dirs(): bin2data=../share/openocd
Debug: 18 18 configuration.c:42 add_script_search_dir(): adding /root/.openocd
Debug: 19 18 configuration.c:42 add_script_search_dir(): adding /usr/local/bin/../share/openocd/site
Debug: 20 18 configuration.c:42 add_script_search_dir(): adding /usr/local/bin/../share/openocd/scripts
Debug: 21 18 command.c:143 script_debug(): command - ocd_command ocd_command type ocd_log_output openocd.log
Debug: 22 18 command.c:143 script_debug(): command - log_output ocd_log_output openocd.log
Debug: 24 18 configuration.c:82 find_file(): found altera-usb-blaster.cfg
Debug: 25 18 command.c:143 script_debug(): command - ocd_command ocd_command type ocd_interface usb_blaster
Debug: 26 18 command.c:143 script_debug(): command - interface ocd_interface usb_blaster
Debug: 28 18 command.c:364 register_command_handler(): registering 'ocd_usb_blaster_device_desc'...
Debug: 29 18 command.c:364 register_command_handler(): registering 'ocd_usb_blaster_vid_pid'...
Debug: 30 18 command.c:364 register_command_handler(): registering 'ocd_usb_blaster_lowlevel_driver'...
Debug: 31 18 command.c:364 register_command_handler(): registering 'ocd_usb_blaster_pin'...
Debug: 32 18 command.c:364 register_command_handler(): registering 'ocd_usb_blaster_firmware'...
Warn : 33 18 adapter.c:159 handle_interface_command(): Adapter driver 'usb_blaster' did not declare which transports it allows; assuming legacy JTAG-only
Info : 34 18 transport.c:117 allow_transports(): only one transport option; autoselect 'jtag'
Debug: 35 18 command.c:364 register_command_handler(): registering 'ocd_jtag_flush_queue_sleep'...
Debug: 36 18 command.c:364 register_command_handler(): registering 'ocd_jtag_rclk'...
Debug: 37 18 command.c:364 register_command_handler(): registering 'ocd_jtag_ntrst_delay'...
Debug: 38 18 command.c:364 register_command_handler(): registering 'ocd_jtag_ntrst_assert_width'...
Debug: 39 18 command.c:364 register_command_handler(): registering 'ocd_scan_chain'...
Debug: 40 18 command.c:364 register_command_handler(): registering 'ocd_jtag_reset'...
Debug: 41 18 command.c:364 register_command_handler(): registering 'ocd_runtest'...
Debug: 42 18 command.c:364 register_command_handler(): registering 'ocd_irscan'...
Debug: 43 18 command.c:364 register_command_handler(): registering 'ocd_verify_ircapture'...
Debug: 44 18 command.c:364 register_command_handler(): registering 'ocd_verify_jtag'...
Debug: 45 18 command.c:364 register_command_handler(): registering 'ocd_tms_sequence'...
Debug: 46 18 command.c:364 register_command_handler(): registering 'ocd_wait_srst_deassert'...
Debug: 47 18 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 48 18 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 49 18 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 50 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 51 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 52 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 53 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 54 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 55 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 56 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 57 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 58 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 59 19 command.c:364 register_command_handler(): registering 'ocd_jtag'...
Debug: 60 19 command.c:364 register_command_handler(): registering 'ocd_svf'...
Debug: 61 19 command.c:364 register_command_handler(): registering 'ocd_xsvf'...
Debug: 62 19 command.c:143 script_debug(): command - ocd_command ocd_command type ocd_init
Debug: 63 19 command.c:143 script_debug(): command - init ocd_init
Debug: 65 19 command.c:143 script_debug(): command - ocd_command ocd_command type ocd_target init
Debug: 66 19 command.c:143 script_debug(): command - ocd_target ocd_target init
Debug: 68 19 command.c:143 script_debug(): command - ocd_command ocd_command type ocd_target names
Debug: 69 19 command.c:143 script_debug(): command - ocd_target ocd_target names
Debug: 70 19 target.c:1329 handle_target_init_command(): Initializing targets...
Info : 71 19 usb_blaster.c:854 ublast_init(): No lowlevel driver configured, will try them all
Info : 72 25 ublast2_access_libusb.c:231 ublast2_libusb_init(): Altera USB-Blaster II found (Firm. rev. = )
Info : 73 25 core.c:1357 adapter_init(): This adapter doesn't support configurable speed
Debug: 74 25 openocd.c:140 handle_init_command(): Debug Adapter init complete
Debug: 75 25 command.c:143 script_debug(): command - ocd_command ocd_command type ocd_transport init
Debug: 76 25 command.c:143 script_debug(): command - ocd_transport ocd_transport init
Debug: 78 25 transport.c:239 handle_transport_init(): handle_transport_init
What do I do not so?