- Tue Mar 21, 2017 1:16 am
#193995
Dear All
I have a Central Battery System which outputs 240 AC Voltage during normal operation and in case the Central Battery system loses its AC input voltage it will output 220 VDC, i need a circuit that blocks DC Voltage and only output AC because my Exit Light Fittings doesn't accept DC Voltage and it has its own internal battery to make it run during power outage.
The idea of keeping this Exit light fittings to the central battery system is that there is monitor module that will report if the light fittings is not running during normal operation to change it in case it is defected.
I am thinking of using capacitor between the output of the monitor module (v-cg-se 4-400 w) and the Exit light fittings to block the DC Voltage is this right solution and what should be the capacity of the capacitor.
I have a Central Battery System which outputs 240 AC Voltage during normal operation and in case the Central Battery system loses its AC input voltage it will output 220 VDC, i need a circuit that blocks DC Voltage and only output AC because my Exit Light Fittings doesn't accept DC Voltage and it has its own internal battery to make it run during power outage.
The idea of keeping this Exit light fittings to the central battery system is that there is monitor module that will report if the light fittings is not running during normal operation to change it in case it is defected.
I am thinking of using capacitor between the output of the monitor module (v-cg-se 4-400 w) and the Exit light fittings to block the DC Voltage is this right solution and what should be the capacity of the capacitor.