- Mon Mar 20, 2017 6:15 am
#193976
I'm completely new to JTAG and OpenOCD, so sorry if this is a stupid question. Can someone point me towards a suitable OpenOCD configuration for the ATSAM3X8E?
I've got a prototype board we're building with a SAM3X (the ATSAM3X8EA-AU, to be exact) on it, with JTAG pins broken out to a header. I've connected the JTAG pins to a Raspberry Pi as described at https://github.com/synthetos/PiOCD/wiki ... TAG-Dongle. I'm running OpenOCD as:
Can someone point me to towards a suitable configuration for this part, please?
I've got a prototype board we're building with a SAM3X (the ATSAM3X8EA-AU, to be exact) on it, with JTAG pins broken out to a header. I've connected the JTAG pins to a Raspberry Pi as described at https://github.com/synthetos/PiOCD/wiki ... TAG-Dongle. I'm running OpenOCD as:
Code: Select all
and raspberrypi-due.tcl contains this:sudo openocd -s /usr/local/share/openocd -f raspberrypi-due.tcl
Code: Select all
After some initial confusion over the difference between pin numbers and GPIO numbers, now when I try to run OpenOCD, I get this:source [find interface/raspberrypi2-native.cfg]
set _CHIPNAME sam3
source [find target/at91sam3ax_8x.cfg]
$_TARGETNAME configure -event gdb-attach {reset init }
Code: Select all
and this last error is repeated at some length. It seems that the chip is reporting a different identifier to what OpenOCD expects for this part.Open On-Chip Debugger 0.10.0+dev-00093-g6b2acc0 (2017-03-17-16:47)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
BCM2835 GPIO config: tck = 11, tms = 25, tdi = 10, tdo = 9
BCM2835 GPIO nums: swclk = 25, swdio = 24
BCM2835 GPIO config: trst = 7
trst_only separate trst_push_pull
Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'.
adapter speed: 500 kHz
adapter_nsrst_delay: 100
jtag_ntrst_delay: 100
cortex_m reset_config sysresetreq
Info : BCM2835 GPIO JTAG/SWD bitbang driver
Info : JTAG and SWD modes enabled
Info : clock speed 500 kHz
Info : JTAG tap: sam3.cpu tap/device found: 0x05b2b03f (mfg: 0x01f (Atmel), part: 0x5b2b, ver: 0x0)
Warn : JTAG tap: sam3.cpu UNEXPECTED: 0x05b2b03f (mfg: 0x01f (Atmel), part: 0x5b2b, ver: 0x0)
Error: JTAG tap: sam3.cpu expected 1 of 1: 0x4ba00477 (mfg: 0x23b (ARM Ltd.), part: 0xba00, ver: 0x4)
Error: Trying to use configured scan chain anyway...
Error: sam3.cpu: IR capture error; saw 0x09 not 0x01
Warn : Bypassing JTAG setup events due to errors
Error: Invalid ACK (7) in DAP response
Error: JTAG-DP STICKY ERROR
Error: Invalid ACK (7) in DAP response
Error: JTAG-DP STICKY ERROR
Can someone point me to towards a suitable configuration for this part, please?