- Fri Mar 17, 2017 5:07 pm
#193949
Hi, I recently bought the Sparkfun MPU-9250 and hooked it up to my arduino mega but I think im doing something wrong. Loading up the MPU9250BasicAHRS_I2C example script and uploading I get this in the serial monitor.
Code: Select all
I'm new to this but I was hoping there was a working example to learn and build myself up from. Can anyone share a tip on what I should do?MPU9250 I AM 0x71 I should be 0x71
MPU9250 is online...
BHW::ii = 0
BHW::ii = 1
BHW::ii = 2
//This repeats till 199, saving thread space.
BHW::ii = 199
x-axis self test: acceleration trim within : 2.7% of factory value
y-axis self test: acceleration trim within : -0.6% of factory value
z-axis self test: acceleration trim within : 2.0% of factory value
x-axis self test: gyration trim within : -4.7% of factory value
y-axis self test: gyration trim within : -1.0% of factory value
z-axis self test: gyration trim within : 0.9% of factory value
MPU9250 initialized for active data mode....
AK8963 I AM 0xFF I should be 0x48
Communication failed, abort!