[phpBB Debug] PHP Warning: in file /mnt/forum-shared/ext/sitesplat/BBCore/event/listener.php on line 70: in_array() expects parameter 2 to be array, boolean given
Optocoupler Circuit Overheating - SparkFun Electronics

SparkFun Forums 

Where electronics enthusiasts find answers.

Questions relating to designing PCBs
By djjohnson70
#191527
I must be missing something. I tried to design a simple Optocoupler circuit. I have a 24V power supply which powers a 7805 Voltage Regulator. A simple switch powers the Optocoupler. I have a delay timer (555 timer) in between the input and the output Optocouplers.

I put this on a breadboard, but when I leave the input pushbutton pressed, the 7805 Voltage regulator gets very hot, very quickly. The circuit performs the function that I expect, but I didn't think I would draw that much current, as the 7805 is rated for 1.5A.

What can be drawing so much current that the regulator cannot supply the required voltage? What have I messed up in this circuit?

The attached image shows the circuit. NOTE: Everything in orange is the bottom layer of the PCB design, which is all ground.

DJ
You do not have the required permissions to view the files attached to this post.
By skimask
#191529
Yep, operating completely normally.
So...how much current is your circuit pulling from the 24v source?
7805 hmmmm...
READ the datasheet, the whole datasheet, top to bottom, then READ it again.
So far you didn't really mess up anything in the circuit, just in your overall assumptions on how things should work vs. how they actually work.
By davep238
#191533
The 555 timer's power supply can be up to 16 volts, so why not use a 12 volt regulator (7812) instead of the 5 volt one? The 7812 will dissipate less heat since there will only be a 12 volt drop across it vs 19. A small heat sink would be a good idea too.