- Sun Feb 14, 2016 3:51 am
#188140
Tomadevil wrote:Yes I do receive messages on the serial monitor, but that doesn't necessarily mean it is working properly.Correct. But if someone only says "it doesn't work" without other explanation of what it IS doing, meaning any signs of life, then we have to assume even the worst of conditions are possible. That the microcontroller is dead or damaged, has a power supply failure or short in it's supply circuit, is in a reset-state, or got itself locked in a program state without ever having done any change to it's GPIO pins. A full explanation of it's behaviour is essential in locating the source of an issue. "doesn't work" doesn't help.
I'm sorry, you are right. I should have mentioned that this is running on an Arduino UNO. You can see how I connected it to the arduino here, and yes I have pull up resistors in circuit:Good
http://www.robot-electronics.co.uk/htm/ ... PS11%20I2C
Yes I do receive messages on the serial monitor...Which are? Again, we have to know what it is thinking or doing, or where it takes the wrong action.