- Thu Nov 19, 2015 8:07 am
#186028
Hallo guys,
I'm new in this Forum.
I have a problem with flashing my Freescale, Openocd does not complete the inti-command.
Openocd failt by reading or writing in the memory for Private Peripheral Bus.
At each try it's an other adress, but some adresses are read- oder writeable.
The error-message look like this error:
Here my Config-File:
EDIT: Sometimes the init finished without errors
Regards,
Samuel
I'm new in this Forum.
I have a problem with flashing my Freescale, Openocd does not complete the inti-command.
Openocd failt by reading or writing in the memory for Private Peripheral Bus.
At each try it's an other adress, but some adresses are read- oder writeable.
The error-message look like this error:
Code: Select all
Open On-Chip Debugger 0.9.0-rc1 (2015-04-24-22:05)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : FTDI SWD mode enabled
Info : add flash_bank kinetis MKL16Z128VFM4.flash
adapter speed: 1000 kHz
none separate
cortex_m reset_config sysresetreq
Info : clock speed 1000 kHz
Info : SWD IDCODE 0x0bc11477
Info : SWD IDCODE 0x0bc11477
Error: Failed to read memory at 0xe000ed00
Polling target MKL16Z128VFM4.cpu failed, trying to reexamine
Info : SWD IDCODE 0x0bc11477
Info : SWD IDCODE 0x0bc11477
Error: Failed to write memory at 0xe0001028
Info : MKL16Z128VFM4.cpu: hardware has 2 breakpoints, 2 watchpoints
Error: The 'check_security' command must be used after 'init'.
in procedure 'init' called at file "D:\Eclipse\Workspace\We******Samuel\Demozuspieler\MKL16Z4.cfg", line 86
in procedure 'ocd_bouncer'
in procedure 'nand'
in procedure 'ocd_bouncer'
Polling target MKL16Z128VFM4.cpu failed, trying to reexamine
Info : SWD IDCODE 0x0bc11477
Info : SWD IDCODE 0x0bc11477
Error: Failed to read memory at 0xe000edfc
Info : MKL16Z128VFM4.cpu: hardware has 0 breakpoints, 2 watchpoints
Error: The 'check_security' command must be used after 'init'.
in procedure 'init' called at file "D:\Eclipse\Workspace\We******Samuel\Demozuspieler\MKL16Z4.cfg", line 86
in procedure 'ocd_bouncer'
in procedure 'pld'
in procedure 'ocd_bouncer'
Polling target MKL16Z128VFM4.cpu failed, trying to reexamine
Info : SWD IDCODE 0x0bc11477
Info : MKL16Z128VFM4.cpu: hardware has 2 breakpoints, 2 watchpoints
Warn : *********** ATTENTION! ATTENTION! ATTENTION! ATTENTION! **********
Warn : **** ****
Warn : **** Your Kinetis MCU is in secured state, which means that, ****
Warn : **** with exception for very basic communication, JTAG/SWD ****
Warn : **** interface will NOT work. In order to restore its ****
Warn : **** functionality please issue 'kinetis mdm mass_erase' ****
Warn : **** command, power cycle the MCU and restart OpenOCD. ****
Warn : **** ****
Warn : *********** ATTENTION! ATTENTION! ATTENTION! ATTENTION! **********
shutdown command invoked
Here my Config-File:
Code: Select all
I hope someone here can help me #
# Freescale Kinetis KL series devices
#
interface ftdi
ftdi_device_desc "FT2232H MiniModule"
ftdi_vid_pid 0x0403 0x6010
ftdi_layout_init 0x0028 0x00eb
#ftdi_layout_init 0x00a8 0x00eb
#ftdi_layout_signal nSRST -noe 0x0020
ftdi_layout_signal SWD_EN -ndata 0x0080
ftdi_layout_signal SWDIO_OE -data 0x0008
set ENDIAN little
set _CHIPNAME MKL16Z128VFM4
transport select swd
source [find target/swj-dp.tcl]
# Work-area is a space in RAM used for flash programming
# By default use 4kB
if { [info exists WORKAREASIZE] } {
set _WORKAREASIZE $WORKAREASIZE
} else {
set _WORKAREASIZE 0x1000
}
if { [info exists CPUTAPID] } {
set _CPUTAPID $CPUTAPID
} else {
set _CPUTAPID 0x0bc11477
}
swj_newdap $_CHIPNAME cpu -irlen 4 -expected-id $_CPUTAPID
set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME cortex_m -chain-position $_CHIPNAME.cpu -endian little
# It is important that "kinetis mdm check_security" is called for
# 'examine-end' event and not 'eximine-start'. Calling it in 'examine-start'
# causes "kinetis mdm check_security" to fail the first time openocd
# calls it when it tries to connect after the CPU has been power-cycled.
$_CHIPNAME.cpu configure -event examine-end {
kinetis mdm check_security
}
$_TARGETNAME configure -work-area-phys 0x20000000 -work-area-size $_WORKAREASIZE
set _FLASHNAME $_CHIPNAME.flash
#flash bank $_FLASHNAME kinetis 0 131072 0 0 $_TARGETNAME
flash bank $_FLASHNAME kinetis 0 0x08000000 0 0 $_TARGETNAME
#flash banks
# Table 5-1. Clock Summary of KL25 Sub-Family Reference Manual
# specifies up to 1MHz for VLPR mode.
adapter_khz 1000
#debug_level 3
#reset_config srst_nogate
#reset_config srst_only
reset_config none
cortex_m reset_config sysresetreq
#targets
#if {![using_hla]} {
# if srst is not fitted use SYSRESETREQ to
# perform a soft reset
# cortex_m reset_config sysresetreq
#}
$_TARGETNAME configure -event reset-init {
# Table 5-1. Clock Summary of KL25 Sub-Family Reference Manual
# specifies up to 24MHz for run mode; Table 17 of Sub-Family Data
# Sheet rev4 lists 25MHz as the maximum frequency.
adapter_khz 24000
}
#commands for flashing
init
#reset halt
#kinetis mdm test_securing
#kinetis mdm check_security
#kinetis mdm check_security
#flash probe 0
#kinetis mdm mass_erase
#flash write_image D:/Eclipse/Workspace/We******Samuel/Demozuspieler/Debug/Demozuspieler.hex 0 ihex
#reset run
shutdown

EDIT: Sometimes the init finished without errors
Regards,
Samuel