- Wed Dec 17, 2014 7:59 am
#177818
Hi, I think it's time I invest in an oscilloscope. Picking one is turning into a devil of a choice.
From what I can tell, there are two basic styles, one is a conventional desktop model with integrated screen (like Sparkfun sells), the other is a USB style, which uses the PC's screen. It is possible that I will want to use this where I do not have access to AC power. The GA1102CAL, which looks like a nice product, requires AC power. That adds to the bucket list should I ever want to operate it portable (inverter, 12V source, etc). The USB powered scope (Hantek, et al) draws power from the USB bus. So plugging it into the USB on a laptop seems like a way to do portable operations.
The two concerns I have are the current draw from USB (not documented that I can find) and the notation in the Hantek documents that the PC should be grounded (presumably to limit noise from a floating power source). Does anyone have any thoughts on either of these concerns ?
From what I can tell, there are two basic styles, one is a conventional desktop model with integrated screen (like Sparkfun sells), the other is a USB style, which uses the PC's screen. It is possible that I will want to use this where I do not have access to AC power. The GA1102CAL, which looks like a nice product, requires AC power. That adds to the bucket list should I ever want to operate it portable (inverter, 12V source, etc). The USB powered scope (Hantek, et al) draws power from the USB bus. So plugging it into the USB on a laptop seems like a way to do portable operations.
The two concerns I have are the current draw from USB (not documented that I can find) and the notation in the Hantek documents that the PC should be grounded (presumably to limit noise from a floating power source). Does anyone have any thoughts on either of these concerns ?
First learned EE at the juncture of vacuum tubes and solid state, Still learning.