- Sat Mar 01, 2014 8:36 am
#168985
Hi,
I'm still a bit of a newbie, so forgive me if this is an obvious question.
I'm trying to use the XSTANDBY pin on a Copernicus II module to put the module into standby (low power) mode. According to the manual, "This logic level input is used to control the RUN/STANDBY state of the module. If this signal is High, the unit will run normally. If this signal is Low, the unit will go to “STANDBY” mode." Easy enough.
Now, I'm powering the GPS module through a Breadboard power supply stick (at 3.3v of course), so I'm thinking that I should just be able to connect the XSTANDBY pin to ground. However, when I do that the power indicator LED on my power supply stick blinks off, which suggests trouble to me. Sure enough, my DMM shows a short between the VCC and XSTANDBY pins on the GPS module (with the module complete disconnected from anything else).
My newbie question is: is this normal for this module or does this suggest it's broken? I've soldered in some header pins, but I'm quite sure my soldering job is okay. The schematic also shows a solder jumper between VCC and XSTANDBY, but I haven't touched it, and it looks good (i.e., open) to me.
I'm still a bit of a newbie, so forgive me if this is an obvious question.
I'm trying to use the XSTANDBY pin on a Copernicus II module to put the module into standby (low power) mode. According to the manual, "This logic level input is used to control the RUN/STANDBY state of the module. If this signal is High, the unit will run normally. If this signal is Low, the unit will go to “STANDBY” mode." Easy enough.
Now, I'm powering the GPS module through a Breadboard power supply stick (at 3.3v of course), so I'm thinking that I should just be able to connect the XSTANDBY pin to ground. However, when I do that the power indicator LED on my power supply stick blinks off, which suggests trouble to me. Sure enough, my DMM shows a short between the VCC and XSTANDBY pins on the GPS module (with the module complete disconnected from anything else).
My newbie question is: is this normal for this module or does this suggest it's broken? I've soldered in some header pins, but I'm quite sure my soldering job is okay. The schematic also shows a solder jumper between VCC and XSTANDBY, but I haven't touched it, and it looks good (i.e., open) to me.