I tend to agree with the previous poster. I attach here some arduino code that runs well on my 328P but gives silly temperature values. Its worth trying though . If you get a good temperature please post corrected code .
Code: Select all/*
MPL115A1 SPI Digital Barometer Test Code
Created on: September 30, 2010
By: Jeremiah McConnell - miah at miah.com
Portions: Jim Lindblom - jim at sparkfun.com
This is a simple test program for the MPL115A1 Pressure Sensor (SPI version).
Hardware: ATmega168, ATmega328
Powered at 3.3V or 5V, running at 8MHz or 16MHz.
MPL115A1 Breakout ------------- Arduino
----------------- -------
SDN ------------------- D9
CSN ------------------- D10
SDO ------------------- D12 *
SDI ------------------- D11 *
SCK ------------------- D13 *
GND ------------------- GND
VDD ------------------- VCC +
* These pins physically connect to the SPI device so you can't change them
+ 5V board use 5V VDD, 3.3V board use 3.3V VDD
License: CCAv3.0 Attribution-ShareAlike (http://creativecommons.org/licenses/by-sa/3.0/)
You're free to use this code for any venture, but I'd love to hear about what you do with it,
and any awesome changes you make to it. Attribution is greatly appreciated.
*/
// Includes
#include <SPI.h>
// Get your current altimiter setting from from the National
// Weather Service - http://www.weather.gov
// This value is often labeled "Barometer" or "Barometric Pressure" or just "Pressure"
#define NWS_BARO 29.92
// Pin definitions
#define MPL115A1_ENABLE_PIN 9
#define MPL115A1_SELECT_PIN 10
// Masks for MPL115A1 SPI i/o
#define MPL115A1_READ_MASK 0x80
#define MPL115A1_WRITE_MASK 0x7F
// MPL115A1 register address map
#define PRESH 0x00 // 80
#define PRESL 0x02 // 82
#define TEMPH 0x04 // 84
#define TEMPL 0x06 // 86
#define A0MSB 0x08 // 88
#define A0LSB 0x0A // 8A
#define B1MSB 0x0C // 8C
#define B1LSB 0x0E // 8E
#define B2MSB 0x10 // 90
#define B2LSB 0x12 // 92
#define C12MSB 0x14 // 94
#define C12LSB 0x16 // 96
#define C11MSB 0x18 // 98
#define C11LSB 0x1A // 9A
#define C22MSB 0x1C // 9C
#define C22LSB 0x1E // 9E
// Unit conversion macros
#define FT_TO_M(x) ((long)((x)*(0.3048)))
#define KPA_TO_INHG(x) ((x)*(0.295333727))
#define KPA_TO_MMHG(x) ((x)*(7.50061683))
#define KPA_TO_PSIA(x) ((x)*(0.145037738))
#define KPA_TO_KGCM2(x) ((x)*(0.0102))
#define INHG_TO_PSIA(x) ((x)*(0.49109778))
#define DEGC_TO_DEGF(x) ((x)*(9.0/5.0)+32)
void setup() {
// initialize serial i/o
Serial.begin(9600);
// initialize SPI interface
SPI.begin();
// these are the defaults
//SPI.setDataMode(SPI_MODE0);
//SPI.setClockDivider(SPI_CLOCK_DIV4); // MPL115A1 supports up to 8MHz
//SPI.setBitOrder(MSBFIRST);
// initialize the chip select and enable pins
pinMode(MPL115A1_SELECT_PIN, OUTPUT);
pinMode(MPL115A1_ENABLE_PIN, OUTPUT);
// sleep the MPL115A1
digitalWrite(MPL115A1_ENABLE_PIN, LOW);
// set the chip select inactive, select signal is CS LOW
digitalWrite(MPL115A1_SELECT_PIN, HIGH);
// spam welcome banner
Serial.print("\n************************************************************************************\n");
Serial.print("* Using Altimiter Setting: ");
Serial.print(NWS_BARO, 2);
Serial.print(" in Hg *\n");
Serial.print("* Visit http://www.weather.gov for your current local value. *\n");
Serial.print("************************************************************************************\n");
}
void loop() {
float pressure_pKa = 0;
float temperature_c= 0;
long altitude_ft = 0;
// wake the MPL115A1
digitalWrite(MPL115A1_ENABLE_PIN, HIGH);
delay(20); // give the chip a few ms to wake up
pressure_pKa = calculatePressurekPa();
temperature_c = calculateTemperatureC();
altitude_ft = calculateAltitudeFt(pressure_pKa);
// put the MPL115A1 to sleep, it has this feature why not use it
// while in shutdown the part draws ~1uA
digitalWrite(MPL115A1_ENABLE_PIN, LOW);
// print table of altitude, pressures, and temperatures to console
Serial.print(altitude_ft);
Serial.print(" ft | ");
Serial.print(FT_TO_M(altitude_ft));
Serial.print(" m | ");
Serial.print(KPA_TO_INHG(pressure_pKa), 2);
Serial.print(" in Hg | ");
Serial.print(KPA_TO_MMHG(pressure_pKa), 0);
Serial.print(" mm Hg | ");
Serial.print(KPA_TO_PSIA(pressure_pKa), 2);
Serial.print(" psia | ");
//Serial.print(KPA_TO_KGCM2(pressure_pKa), 3);
///Serial.print(" kg/cm2 | ");
Serial.print(pressure_pKa, 1);
Serial.print(" kPa | ");
// At a res of -5.35 counts/°C, digits lower than 0.1°C are not significant
Serial.print(temperature_c, 1);
Serial.print(" C | ");
Serial.print(DEGC_TO_DEGF(temperature_c), 1);
Serial.print(" F\n");
// wait a few seconds before looping
delay(5000);
}
long calculateAltitudeFt(float pressure_kPa) {
float delta;
long altitude_ft;
// See http://en.wikipedia.org/wiki/Barometric_formula
// If you're a pilot you need to know what's going on here,
// otherwise just know these steps calculate the barometric altitude (ft)
// based on the ratio of absolute barometric pressure (psia) to the
// altimiter setting (psia).
delta = KPA_TO_PSIA(pressure_kPa) / INHG_TO_PSIA( NWS_BARO );
altitude_ft = (1 - pow(delta, (1 / 5.25587611))) / 0.0000068756;
return altitude_ft;
}
float calculateTemperatureC() {
unsigned int uiTadc;
unsigned char uiTH, uiTL;
unsigned int temperature_counts = 0;
writeRegister(0x22, 0x00); // Start temperature conversion
delay(2); // Max wait time is 0.7ms, typ 0.6ms
// Read pressure
uiTH = readRegister(TEMPH);
uiTL = readRegister(TEMPL);
uiTadc = (unsigned int) uiTH << 8;
uiTadc += (unsigned int) uiTL & 0x00FF;
// Temperature is a 10bit value
uiTadc = uiTadc >> 6;
// -5.35 counts per °C, 472 counts is 25°C
return 25 + (uiTadc - 472) / -5.35;
}
float calculatePressurekPa() {
// See Freescale document AN3785 for detailed explanation
// of this implementation.
signed char sia0MSB, sia0LSB;
signed char sib1MSB, sib1LSB;
signed char sib2MSB, sib2LSB;
signed char sic12MSB, sic12LSB;
signed char sic11MSB, sic11LSB;
signed char sic22MSB, sic22LSB;
signed int sia0, sib1, sib2, sic12, sic11, sic22, siPcomp;
float decPcomp;
signed long lt1, lt2, lt3, si_c11x1, si_a11, si_c12x2;
signed long si_a1, si_c22x2, si_a2, si_a1x1, si_y1, si_a2x2;
unsigned int uiPadc, uiTadc;
unsigned char uiPH, uiPL, uiTH, uiTL;
writeRegister(0x24, 0x00); // Start Both Conversions
//writeRegister(0x20, 0x00); // Start Pressure Conversion
//writeRegister(0x22, 0x00); // Start temperature conversion
delay(2); // Max wait time is 1ms, typ 0.8ms
// Read pressure
uiPH = readRegister(PRESH);
uiPL = readRegister(PRESL);
uiTH = readRegister(TEMPH);
uiTL = readRegister(TEMPL);
uiPadc = (unsigned int) uiPH << 8;
uiPadc += (unsigned int) uiPL & 0x00FF;
uiTadc = (unsigned int) uiTH << 8;
uiTadc += (unsigned int) uiTL & 0x00FF;
// Placing Coefficients into 16-bit Variables
// a0
sia0MSB = readRegister(A0MSB);
sia0LSB = readRegister(A0LSB);
sia0 = (signed int) sia0MSB << 8;
sia0 += (signed int) sia0LSB & 0x00FF;
// b1
sib1MSB = readRegister(B1MSB);
sib1LSB = readRegister(B1LSB);
sib1 = (signed int) sib1MSB << 8;
sib1 += (signed int) sib1LSB & 0x00FF;
// b2
sib2MSB = readRegister(B2MSB);
sib2LSB = readRegister(B2LSB);
sib2 = (signed int) sib2MSB << 8;
sib2 += (signed int) sib2LSB & 0x00FF;
// c12
sic12MSB = readRegister(C12MSB);
sic12LSB = readRegister(C12LSB);
sic12 = (signed int) sic12MSB << 8;
sic12 += (signed int) sic12LSB & 0x00FF;
// c11
sic11MSB = readRegister(C11MSB);
sic11LSB = readRegister(C11LSB);
sic11 = (signed int) sic11MSB << 8;
sic11 += (signed int) sic11LSB & 0x00FF;
// c22
sic22MSB = readRegister(C22MSB);
sic22LSB = readRegister(C22LSB);
sic22 = (signed int) sic22MSB << 8;
sic22 += (signed int) sic22LSB & 0x00FF;
// Coefficient 9 equation compensation
uiPadc = uiPadc >> 6;
uiTadc = uiTadc >> 6;
// Step 1 c11x1 = c11 * Padc
lt1 = (signed long) sic11;
lt2 = (signed long) uiPadc;
lt3 = lt1*lt2;
si_c11x1 = (signed long) lt3;
// Step 2 a11 = b1 + c11x1
lt1 = ((signed long)sib1)<<14;
lt2 = (signed long) si_c11x1;
lt3 = lt1 + lt2;
si_a11 = (signed long)(lt3>>14);
// Step 3 c12x2 = c12 * Tadc
lt1 = (signed long) sic12;
lt2 = (signed long) uiTadc;
lt3 = lt1*lt2;
si_c12x2 = (signed long)lt3;
// Step 4 a1 = a11 + c12x2
lt1 = ((signed long)si_a11<<11);
lt2 = (signed long)si_c12x2;
lt3 = lt1 + lt2;
si_a1 = (signed long) lt3>>11;
// Step 5 c22x2 = c22*Tadc
lt1 = (signed long)sic22;
lt2 = (signed long)uiTadc;
lt3 = lt1 * lt2;
si_c22x2 = (signed long)(lt3);
// Step 6 a2 = b2 + c22x2
lt1 = ((signed long)sib2<<15);
lt2 = ((signed long)si_c22x2>1);
lt3 = lt1+lt2;
si_a2 = ((signed long)lt3>>16);
// Step 7 a1x1 = a1 * Padc
lt1 = (signed long)si_a1;
lt2 = (signed long)uiPadc;
lt3 = lt1*lt2;
si_a1x1 = (signed long)(lt3);
// Step 8 y1 = a0 + a1x1
lt1 = ((signed long)sia0<<10);
lt2 = (signed long)si_a1x1;
lt3 = lt1+lt2;
si_y1 = ((signed long)lt3>>10);
// Step 9 a2x2 = a2 * Tadc
lt1 = (signed long)si_a2;
lt2 = (signed long)uiTadc;
lt3 = lt1*lt2;
si_a2x2 = (signed long)(lt3);
// Step 10 pComp = y1 + a2x2
lt1 = ((signed long)si_y1<<10);
lt2 = (signed long)si_a2x2;
lt3 = lt1+lt2;
// Fixed point result with rounding
//siPcomp = ((signed int)lt3>>13);
siPcomp = lt3/8192;
// decPcomp is defined as a floating point number
// Conversion to decimal value from 1023 ADC count value
// ADC counts are 0 to 1023, pressure is 50 to 115kPa respectively
decPcomp = ((65.0/1023.0)*siPcomp)+50;
return decPcomp;
}
unsigned int readRegister(byte thisRegister) {
byte result = 0;
// select the MPL115A1
digitalWrite(MPL115A1_SELECT_PIN, LOW);
// send the request
SPI.transfer(thisRegister | MPL115A1_READ_MASK);
result = SPI.transfer(0x00);
// deselect the MPL115A1
digitalWrite(MPL115A1_SELECT_PIN, HIGH);
return result;
}
void writeRegister(byte thisRegister, byte thisValue) {
// select the MPL115A1
digitalWrite(MPL115A1_SELECT_PIN, LOW);
// send the request
SPI.transfer(thisRegister & MPL115A1_WRITE_MASK);
SPI.transfer(thisValue);
// deselect the MPL115A1
digitalWrite(MPL115A1_SELECT_PIN, HIGH);
}