- Sat Dec 08, 2012 10:22 pm
#152980
Hello everyone!
I have a question about a robot I am currently in the design stage on. I have been monitoring the voltage requirements of the components I will be using and the amperes of each item. Currently, the project is going to require 3 seperate batteries, 6v, 9v, and 12v. The highest amperes needed are from the Sabertooth motor driver, 2x5 RC, requiring 5A continuous per channel, 10A peak. I was wondering if anyone has a suggestion, or schematic from a previous build, to create a board to supply each of the voltages from a single battery? I need to run a single 24v battery because of weight and space requirements.
My idea is to have either a 14.8, 18, or 24 volt battery which will then run through this board and supply 12v 10A (for the Sabertooth), 9v for both Lynxmotion's Botboarduino and the SSC-32 (Both would need 35-50mA each), and 6v to run all the servos (Hitec servos - 3x HS-422, 3x HS-485HB, & 8x HS-645MG). I figured I would be safe with 12v 10A, 9v 1A, and 6v 5A.
So far, I have this in mind for the curcuit:
LM7809 for 9v (Mouser # 512-LM7809CT)
LM338T for 6v (Mouser # 926-LM338T/NOPB)
LM3150 for 12v 10A (Mouser # 926-LM338T/NOPB)
My only unknown is the LM3150. I personally have never used this chip. Is there another chip anyone would recommend to step-down the 24v to 12v 10A? Better yet, is there a different circuit anyone would recommend over this entirely? Any help, suggestions, tips would be greatly appreciated! If anyone needs any other information or has questions about my circuit I'll be more than happy to answer. I'm really trying to get this circuit built fairly quickly to have it tested prior to installation.
Thank you!
I have a question about a robot I am currently in the design stage on. I have been monitoring the voltage requirements of the components I will be using and the amperes of each item. Currently, the project is going to require 3 seperate batteries, 6v, 9v, and 12v. The highest amperes needed are from the Sabertooth motor driver, 2x5 RC, requiring 5A continuous per channel, 10A peak. I was wondering if anyone has a suggestion, or schematic from a previous build, to create a board to supply each of the voltages from a single battery? I need to run a single 24v battery because of weight and space requirements.
My idea is to have either a 14.8, 18, or 24 volt battery which will then run through this board and supply 12v 10A (for the Sabertooth), 9v for both Lynxmotion's Botboarduino and the SSC-32 (Both would need 35-50mA each), and 6v to run all the servos (Hitec servos - 3x HS-422, 3x HS-485HB, & 8x HS-645MG). I figured I would be safe with 12v 10A, 9v 1A, and 6v 5A.
So far, I have this in mind for the curcuit:
LM7809 for 9v (Mouser # 512-LM7809CT)
LM338T for 6v (Mouser # 926-LM338T/NOPB)
LM3150 for 12v 10A (Mouser # 926-LM338T/NOPB)
My only unknown is the LM3150. I personally have never used this chip. Is there another chip anyone would recommend to step-down the 24v to 12v 10A? Better yet, is there a different circuit anyone would recommend over this entirely? Any help, suggestions, tips would be greatly appreciated! If anyone needs any other information or has questions about my circuit I'll be more than happy to answer. I'm really trying to get this circuit built fairly quickly to have it tested prior to installation.
Thank you!