- Wed Aug 15, 2012 6:41 am
#148497
Has anyone tried the new S3B version (Part no. XBP9B-XC...) of the Pro XSC ? It has extended range, less current draw, but otherwise is supposed to be pin and RF compatible with the older model that Sparkfun is still selling (XBP09-XC...).
Anyway, I purchased one from Digi and dropped it in, in place of the older model of which I have two. It kinda works. I can Test/ Query it in X-CTU with the module connected via Sparkfun XBEE Exploreer USB, and get an OK. But under the modem configuration tab, I am unable to read parameters. When I try to read parameters I get communication errors and it says modem config file not found and other stuff. I Downloaded version updates to X-CTU and still have the same problem. Also, on the X-CTU terminal window I am recieving an incrementing 8 character word scrolling up the screen, when I am not expecting to receive any data at all.
I can send data back and forth between the older model connected to the Explorer USB and the S3B conected to a SF XBEE Regulated Explorer over the air, but data is sporadic and only partially coming through.
Does anyone have one working communicating with SF XBEE Explorers and the older model?
Anyway, I purchased one from Digi and dropped it in, in place of the older model of which I have two. It kinda works. I can Test/ Query it in X-CTU with the module connected via Sparkfun XBEE Exploreer USB, and get an OK. But under the modem configuration tab, I am unable to read parameters. When I try to read parameters I get communication errors and it says modem config file not found and other stuff. I Downloaded version updates to X-CTU and still have the same problem. Also, on the X-CTU terminal window I am recieving an incrementing 8 character word scrolling up the screen, when I am not expecting to receive any data at all.
I can send data back and forth between the older model connected to the Explorer USB and the S3B conected to a SF XBEE Regulated Explorer over the air, but data is sporadic and only partially coming through.
Does anyone have one working communicating with SF XBEE Explorers and the older model?