- Thu Jun 28, 2012 11:04 am
#146737
Hello,
i am new to STM32 controller and i am using a STM32f0 discovery kit. i have been trying to use the interrupt but whenever i generate the external interrupt the controller stops working and freezes while actually nothing should happen because i have defined nothing . this is the code that i wrote for the controller.
#include "stm32f0xx_gpio.h"
#include "stm32f0xx_rcc.h"
#include "stm32f0xx_spi.h"
#include "stm32f0xx_exti.h"
#include "stm32f0xx_syscfg.h"
#include "stm32f0xx_tim.h"
int k =1;
void delay(int a)
{
int b = 500;
a= a*100;
while (a>0)
{
while(b >0)
{b--;}
a--;
}
int sysinit()
{
NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef demo;
SPI_InitTypeDef spicon;
EXTI_InitTypeDef EXTI_InitStructure;
// this function initializes clocks to the ports and defines which ports are inputs and outputs
RCC_DeInit();
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA|RCC_AHBPeriph_GPIOB |RCC_AHBPeriph_GPIOC , ENABLE);
//sending clock to a b c ports
//i think i should initialize the spi1 clock too
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);//clock to spi1 module
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);// clock to gp timer2
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);// dont know but clock has to be sent here
// interrupt settings
EXTI_ClearITPendingBit(EXTI_Line0);
EXTI_InitStructure.EXTI_Line = EXTI_Line0 ;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
// connecting GPIOA) with EXTI1
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0);
// Prioritising interrupt below
NVIC_InitStructure.NVIC_IRQChannel = EXTI0_1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
// GPIO settings
demo.GPIO_Mode = GPIO_Mode_AF;
demo.GPIO_Speed = GPIO_Speed_Level_3;
demo.GPIO_OType = GPIO_OType_PP;
demo.GPIO_PuPd = GPIO_PuPd_DOWN;
demo.GPIO_Pin = GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7; //SPI 1 ports enabled yet spi not initialized
GPIO_Init(GPIOA, &demo);
demo.GPIO_Mode = GPIO_Mode_OUT;
demo.GPIO_Pin = GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3;
GPIO_Init(GPIOA, &demo);// outputs at PA1,2,3
demo.GPIO_Mode = GPIO_Mode_IN;
demo.GPIO_Pin = GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3;
GPIO_Init(GPIOB, &demo);
demo.GPIO_Pin = GPIO_Pin_0;
// defining user button 2 for personal use
GPIO_Init(GPIOA, &demo);
demo.GPIO_Pin = GPIO_Pin_8|GPIO_Pin_9;
demo.GPIO_Mode = GPIO_Mode_OUT;
GPIO_Init(GPIOC, &demo);
//configuring gpio for spi...
GPIO_PinAFConfig(GPIOA,GPIO_PinSource5 |GPIO_PinSource6 |GPIO_PinSource7|GPIO_PinSource4 , GPIO_AF_0);
/// my SPI 1 initialization code for spi master///
spicon.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
spicon.SPI_Mode = SPI_Mode_Master;
spicon.SPI_DataSize = SPI_DataSize_8b;
spicon.SPI_CPOL = SPI_CPOL_High ;
spicon.SPI_CPHA = SPI_CPHA_2Edge;
spicon.SPI_NSS = SPI_NSS_Hard ;
spicon.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_128;
spicon.SPI_FirstBit = SPI_FirstBit_MSB;
spicon.SPI_CRCPolynomial = SPI_CRCLength_8b;
SPI_Init(SPI1, &spicon);
SPI_Cmd(SPI1, ENABLE);
return 0;
}
void EXTI0_1_IRQn_IRQHandler(void)
{
//Check if EXTI_Line1 is asserted
if(EXTI_GetITStatus(EXTI_Line0) != RESET)
{
// do nothing
}
//we need to clear line pending bit manually
EXTI_ClearITPendingBit(EXTI_Line0);
}
int main()
{
sysinit();
while (k)
{
SPI_SendData8(SPI1, 0xAA);
GPIO_SetBits(GPIOC,GPIO_Pin_9);
GPIO_ResetBits(GPIOC,GPIO_Pin_8 );
delay (800);
GPIO_ResetBits(GPIOC,GPIO_Pin_9 );
GPIO_SetBits(GPIOC,GPIO_Pin_8);
SPI_SendData8(SPI1, 0xBA);
delay (800);
}
return 0;
}
i am new to STM32 controller and i am using a STM32f0 discovery kit. i have been trying to use the interrupt but whenever i generate the external interrupt the controller stops working and freezes while actually nothing should happen because i have defined nothing . this is the code that i wrote for the controller.
#include "stm32f0xx_gpio.h"
#include "stm32f0xx_rcc.h"
#include "stm32f0xx_spi.h"
#include "stm32f0xx_exti.h"
#include "stm32f0xx_syscfg.h"
#include "stm32f0xx_tim.h"
int k =1;
void delay(int a)
{
int b = 500;
a= a*100;
while (a>0)
{
while(b >0)
{b--;}
a--;
}
int sysinit()
{
NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef demo;
SPI_InitTypeDef spicon;
EXTI_InitTypeDef EXTI_InitStructure;
// this function initializes clocks to the ports and defines which ports are inputs and outputs
RCC_DeInit();
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA|RCC_AHBPeriph_GPIOB |RCC_AHBPeriph_GPIOC , ENABLE);
//sending clock to a b c ports
//i think i should initialize the spi1 clock too
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);//clock to spi1 module
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);// clock to gp timer2
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);// dont know but clock has to be sent here
// interrupt settings
EXTI_ClearITPendingBit(EXTI_Line0);
EXTI_InitStructure.EXTI_Line = EXTI_Line0 ;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
// connecting GPIOA) with EXTI1
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0);
// Prioritising interrupt below
NVIC_InitStructure.NVIC_IRQChannel = EXTI0_1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
// GPIO settings
demo.GPIO_Mode = GPIO_Mode_AF;
demo.GPIO_Speed = GPIO_Speed_Level_3;
demo.GPIO_OType = GPIO_OType_PP;
demo.GPIO_PuPd = GPIO_PuPd_DOWN;
demo.GPIO_Pin = GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7; //SPI 1 ports enabled yet spi not initialized
GPIO_Init(GPIOA, &demo);
demo.GPIO_Mode = GPIO_Mode_OUT;
demo.GPIO_Pin = GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3;
GPIO_Init(GPIOA, &demo);// outputs at PA1,2,3
demo.GPIO_Mode = GPIO_Mode_IN;
demo.GPIO_Pin = GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3;
GPIO_Init(GPIOB, &demo);
demo.GPIO_Pin = GPIO_Pin_0;
// defining user button 2 for personal use
GPIO_Init(GPIOA, &demo);
demo.GPIO_Pin = GPIO_Pin_8|GPIO_Pin_9;
demo.GPIO_Mode = GPIO_Mode_OUT;
GPIO_Init(GPIOC, &demo);
//configuring gpio for spi...
GPIO_PinAFConfig(GPIOA,GPIO_PinSource5 |GPIO_PinSource6 |GPIO_PinSource7|GPIO_PinSource4 , GPIO_AF_0);
/// my SPI 1 initialization code for spi master///
spicon.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
spicon.SPI_Mode = SPI_Mode_Master;
spicon.SPI_DataSize = SPI_DataSize_8b;
spicon.SPI_CPOL = SPI_CPOL_High ;
spicon.SPI_CPHA = SPI_CPHA_2Edge;
spicon.SPI_NSS = SPI_NSS_Hard ;
spicon.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_128;
spicon.SPI_FirstBit = SPI_FirstBit_MSB;
spicon.SPI_CRCPolynomial = SPI_CRCLength_8b;
SPI_Init(SPI1, &spicon);
SPI_Cmd(SPI1, ENABLE);
return 0;
}
void EXTI0_1_IRQn_IRQHandler(void)
{
//Check if EXTI_Line1 is asserted
if(EXTI_GetITStatus(EXTI_Line0) != RESET)
{
// do nothing
}
//we need to clear line pending bit manually
EXTI_ClearITPendingBit(EXTI_Line0);
}
int main()
{
sysinit();
while (k)
{
SPI_SendData8(SPI1, 0xAA);
GPIO_SetBits(GPIOC,GPIO_Pin_9);
GPIO_ResetBits(GPIOC,GPIO_Pin_8 );
delay (800);
GPIO_ResetBits(GPIOC,GPIO_Pin_9 );
GPIO_SetBits(GPIOC,GPIO_Pin_8);
SPI_SendData8(SPI1, 0xBA);
delay (800);
}
return 0;
}