Wifly Shield + Arduino 1.0

For the discussion of Arduino related topics.

Moderator: phalanx

Post Reply
diripar8
Posts: 4
Joined: Tue Dec 13, 2011 9:18 am

Wifly Shield + Arduino 1.0

Post by diripar8 » Tue Dec 13, 2011 9:22 am

I've been trying to use the library of the Wifly shield with the new 1.0 version of arduino but I could not do it, anyone can help?

Has anyone used the microchip chipkit with wifly shield??

Thanks

avenue33
Posts: 101
Joined: Wed Dec 01, 2010 12:42 pm
Contact:

Re: Wifly Shield + Arduino 1.0

Post by avenue33 » Thu Jan 12, 2012 3:54 am

Yes, but I get rid of the library.

See an example at :arrow: pic32_RTC: the sketch
• acquires date and time from an NTP server using WiFly, and
• updates the chipKIT UNO32 internal RTC (an additional crystal is required).

Enjoy :)

diripar8
Posts: 4
Joined: Tue Dec 13, 2011 9:18 am

Re: Wifly Shield + Arduino 1.0

Post by diripar8 » Mon Jan 23, 2012 8:56 am

Thanks for your help.

satalfa
Posts: 2
Joined: Mon Feb 06, 2012 3:09 pm

Re: Wifly Shield + Arduino 1.0

Post by satalfa » Mon Feb 06, 2012 3:34 pm

Hello,
I've just adapt wifly librarie for a little projet. I've followed the advices of arduino site. My project can build without error, but I don't tested it on a wifly board (I don't have one at this time).
I've replaced Client.h and Server.h by WiFlyClient.h and WiFlyServer.h. And replaced to the classes Client by WiFlyClient and Server by WiFlyServer.
You'll need to change the source of your project to include those new names !
I'm not sure that this will be finallised as "the WiFly librarie for Arduino 1.0", but I suppose it's a good start...

http://dl.free.fr/d8QNZrqdV (right click - save as)

Tell me If this is running...

Bye,
Olivier H

Post Reply