- Tue Jan 18, 2011 1:32 am
#117758
I am having trouble connecting the WiFly board to local WiFi network. I've tried it with security turned on (WPA2) and with it turned off, I keep getting Disconn from acumen4,AUTH-ERR. I am hoping someone can spot something. Here are results of a scan:
So what am I missing here?
Code: Select all
Then I say: join acumen4. I get this in response:SCAN:Found 1
Num SSID Ch RSSI Sec MAC Address Suites
1 acumen4 09 -59 Open 00:0c:41:c2:56:c0 2104 0
Code: Select all
So it seems like it worked, but it did not, because I send show net and get this in response (e.g. DHCP failed):Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..
<2.20>
Disconn from acumen4,AUTH-ERR
Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..
Disconn from acumen4,AUTH-ERR
Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..
Disconn from acumen4,AUTH-ERR
Auto-Assoc acumen4 chan=9 mode=OPEN SCAN OK
Joining acumen4 now..
Associated!
DHCP: Start
Code: Select all
Here are the results of get everything for reference:SSid=acumen4
Chan=9
Assoc=OK
Rate=12, 24Mb
Auth=OK
Mode=OPEN
DHCP=FAIL
Boot=0
Time=OK
Links=1
<2.20>
Code: Select all
I've tried factory reset - did not work. WiFly Ver 2.20, 05-25-2010
Beacon=100
Probe=60
OPEN=*OPEN*
CLOSE=*CLOS*
REMOTE=*HELLO*
FlushSize=900
MatchChar=0
FlushTimer=10
IdleTimer=0
CmdChar=$
IF=DOWN
DHCP=ON
IP=0.0.0.0:2000
NM=0.0.0.0
GW=0.0.0.0
HOST=0.0.0.0:2000
PROTO=TCP,
MTU=1460
FLAGS=0x7
BACKUP=0.0.0.0
DNS=0.0.0.0
Name=server1
Backup=backup2
FTP=208.109.78.34:21
File=wifly-GSX.img
User=roving
Pass=Pass123
SSID=acumen4
Chan=0
ExtAnt=0
Join=1
Auth=OPEN
Mask=0x1fff
Rate=12, 24 Mb
Linkmon=0
Passphrase=rubygirl
SleepTmr=0
WakeTmr=0
Trigger=0x1
Autoconn=0
IoFunc=0x0
IoMask=0x20f0
PrintLvl=0x1
TimeEna=0
TIMEADR=129.6.15.28:123
Zone=7
Baudrate=115200
Flow=0x0
Mode=0x0
JoinTmr=1000
Replace=0x24
DeviceId=WiFly-GSX
Password=
Format=0x0
Sensors=0x0
BCAST=255.255.255.255:55555
Interval=0x7
<2.20>
So what am I missing here?