I mannaged to get the library to compile in EW Kickstart (V4.09A). Unfortunately I get the following error:
*************************************************************
Error[e16]: Segment CSTACK (size: 0x32 align: 0x1) is too long
for segment definition. At least 0x24 more bytes needed. The
problem occurred while processing the segment placement
command "-Z(DATA)CSTACK+_STACK_SIZE#", where at the
moment of placement the available memory ranges were
"CODE:272-27f"
Reserved ranges relevant to this placement:
200-271 DATA16_Z
272-27f CSTACK
Error while running Linker
Total number of errors: 1
Total number of warnings: 0
*************************************************************
which I believe means that it is too large for the device I currently have selected(f2013), which only has 2KB of program flash. TBH, I am not quite sure as I am new to all this.
Does anyone else know? This is something I can really use help with. The only related thing I could find is this:
http://www.embeddedrelated.com/groups/m ... w/8805.php
Happy Tinkering
Bellmar