WiFly Shield code library alpha 2 release

For the discussion of Arduino related topics.

Moderator: phalanx

Re: WiFly Shield code library alpha 2 release

Postby glibdud » Thu Nov 24, 2011 9:41 am

Are there any functions available that you can use to test that the WiFly is still associated with the WLAN? I poked through the source a bit, but didn't see anything obvious. I have it periodically checking a web page, and I'm guessing best practice is to check for association each time I go to hit it so that I can reconnect if necessary. Or does it just auto-reconnect if the connection drops? If so, can I trust that?

Thanks to the author for this library!
glibdud
 
Posts: 1
Joined: Thu Nov 24, 2011 9:36 am

Re: WiFly Shield code library alpha 2 release

Postby Nathalie » Mon Nov 28, 2011 3:46 am

Hi,
Does anyone managed to adapt this library to make it work with the LeafLabs Maple board ?
Thanks for help.

Nathalie
Nathalie
 
Posts: 2
Joined: Mon Nov 28, 2011 2:53 am
Location: Grenoble, France

Re: WiFly Shield code library alpha 2 release

Postby manolinpinguin » Tue Dec 13, 2011 8:05 am

HELP!
I am faily new to all this.
Can anyone tell me how to wire the ?Breakout Board for SC16IS750 I2C/SPI-to-UART IC" to the Wifly Breakout boarld and to arduino?? I should have gotten the Wifly shield but messed up.

Thanks.
manolinpinguin
 
Posts: 1
Joined: Tue Dec 13, 2011 8:02 am

Re: WiFly Shield code library alpha 2 release

Postby goyoregalado » Mon Dec 19, 2011 6:03 pm

I've been using the WiFly Shield library for a while and then I updated to the new Arduino IDE 1.0.
After that the library doesn't compiled anymore.

I've been working on this since yesterday and I believe that I've solved a pair of problems. I can't give any complete guarantee but now I'm using the SPIUartTerminal normally and it works.

The post with the fix is there: http://roostertricopter.blogspot.com/2011/12/sparkfun-wifly-library-alpha-2-fixed.html
goyoregalado
 
Posts: 2
Joined: Mon Dec 19, 2011 5:44 pm

Re: WiFly Shield code library alpha 2 release

Postby cog » Wed Dec 28, 2011 9:11 am

Thank you, trjean and dkflyboy

Your combined posts solved a really confusing issue with my WiFly shield. I was really considering it a waste of time and planned to move to an ethernet shield or wait for the official Arduino wifi shield.

Changing Server.cpp as dkflyboy suggested made my sketch work properly and consistently for the first time after HOURS of work. The additional pointer (that the file to edit is Server.cpp) helped too.

I have an Arduino Uno with a WiFly shield (revision 2) acting as a webserver. It takes a variable from the URL and operates a servo accordingly. It would work some of the time; other times the server would lock it. It would respond to ping OK but the green light would stay on (after a quick flash from the red light) until the browser trying to contact it was closed. A reset button, power cycle or terminal connection (which restarts the sketch) would sometimes solve it, but mostly I had to keep on trying to connect from a browser up to 10 or 20 times before it would start working - and then it would only work some of the time.

I found it difficult to open and edit the CPP file. In the end, I started the IDE then dragged the CPP file into it, save the entire project to the desktop and then copied the new Server.cpp file to the correct location. I also found that renaming the old Server.cpp file to 'Server - old.cpp' doesn't work; it still gets included, resulting in compliation errors. Renaming the file Server.OLD works OK.

Thanks again.
cog
 
Posts: 1
Joined: Wed Dec 28, 2011 9:03 am

Re: WiFly Shield code library alpha 2 release

Postby misfit8d6 » Wed Dec 28, 2011 3:27 pm



Has anyone tested this to confirm and will this be rolled into the official package? Also, looking at the changes above, it doesn't look like the Client/Server have been updated for 1.0 compatibility. Thanks! I'd take a stab at updating everything myself but I don't have a WiFly shield, sorry!
misfit8d6
 
Posts: 6
Joined: Wed Aug 06, 2008 7:45 am

Re: WiFly Shield code library alpha 2 release

Postby bugsworld85 » Thu Dec 29, 2011 4:45 am

Well i modified your server sketch to light up an LED over wifly, but the problem is due to the space restrictions on arduino, i can only place an 'on' and 'off' post button using html to display on the computer browser to operate the LED.

What i really want to do is have a proper website on the computer with the relevant buttons to operate something on the arduino using wifly. Any help would be greatly appreciated.


takha... we have the same project... the only difference is, i am not using SD card shield(whatsoever) and i want to use an android phone to control devices i just wanted to start using a pc to light LEDs... like you, i am also new to this kind of things. i have tried the Page host sketch from the WiFly tutorial and seem to be working fine. the only problem i have is how to make it interactive like working on buttons then pass information to the wifly. it was also introduced on the tutorial, but i wasnt able to understand the last instructions on creating an interactive buttons. could anyone please help with this..
bugsworld85
 
Posts: 3
Joined: Thu Dec 29, 2011 4:35 am

Re: WiFly Shield code library alpha 2 release

Postby goyoregalado » Thu Jan 05, 2012 9:24 am

misfit8d6 wrote:


Has anyone tested this to confirm and will this be rolled into the official package? Also, looking at the changes above, it doesn't look like the Client/Server have been updated for 1.0 compatibility. Thanks! I'd take a stab at updating everything myself but I don't have a WiFly shield, sorry!


I've not used Client/Server but if in two next weeks proably I'll have time to touch that.
I can try to do that but I'll like to know if my modifications works for everyone.

Thanks.
goyoregalado
 
Posts: 2
Joined: Mon Dec 19, 2011 5:44 pm

Re: WiFly Shield code library alpha 2 release

Postby deedrix » Thu Jan 12, 2012 8:56 pm

Hi

I've just begun trying to use the wifly with my Arduino Uno to decipher signal strengths, but before even connecting anything up I attempted to Verify the sketch found in "file > examples > Wifly > tools > SpiUartTerminals" and it has thrown a number of errors with the code.

Code: Select all
SpiUartTerminal.pde:-1: error: 'class SpiUartDevice' has no member named 'print'
SpiUartTerminal.pde:-1: error: 'BYTE' was not declared in this scope


I have not been able to find any forum posts on this error, and surprisingly it never came up in this thread, despite being an initial error before I'd tried anything with it.

Can anybody help?
deedrix
 
Posts: 1
Joined: Thu Jan 12, 2012 8:49 pm

Re: WiFly Shield code library alpha 2 release

Postby egger100 » Mon Jan 16, 2012 12:04 am

Hi

I so far I have been playing around with the WebClient and WebServer examples. I have my own version of the WebClient working and can pull commands from my server successfully. My problem arises after running the client for a few minutes when my client locks up. It appears to enter an infinite loop checking uart.available().

Minimizer seems to have the same issue but I haven't seen any responses yet. Any ideas would be great.

Thanks for the help!
egger100
 
Posts: 2
Joined: Sun Jan 15, 2012 11:56 pm

Re: WiFly Shield code library alpha 2 release

Postby Minimizer » Mon Jan 16, 2012 11:38 pm

Egger -

I haven't followed the thread too closely over the past couple of weeks, but don't believe I've seen any relevant responses related to resolving the occasional hanging problems being encountered. I haven't dug too much more deeply into the library, but believe there are possibly a couple of bugs in there somewhere. The library doesn't appear to be particularly fault tolerant (and the comments included within would indicate the same. This is not a knock on the library at all, and all the good hard work to get it running and posted, just a realization that it's possibly not quite at the stage one would desire it to be at for long-term unattended operation of the WiFly device).

I switched over to using an alternate library, which can be found at ..
http://cairohackerspace.blogspot.com/20 ... g-and.html

To be sure, I've encountered a couple of bugs here too (which I'll admit to having an equally hard time resolving!). My impressions based on some initial testing though is that it may perhaps provide a bit more stable starting point. Good luck with your project.

- Larry (Minimizer)
Minimizer
 
Posts: 9
Joined: Tue Aug 16, 2011 9:05 pm

Re: WiFly Shield code library alpha 2 release

Postby egger100 » Tue Jan 17, 2012 7:35 am

Larry

I was able to track the problem done to the uart stream returning "connection FAILED" instead of "*OPEN*" over time but haven't been able to figure out why or any way around it. I've been looking into other options as well. I don't think I can use the Wifly Serial library you linked because I'm using the full Wifly shield instead of the break out board. I can't easily reroute the RX/TX pins so I'm trying to find another option.

I'll be sure to keep you posted on what I find.

- Reagan (egger100)
egger100
 
Posts: 2
Joined: Sun Jan 15, 2012 11:56 pm

Re: WiFly Shield code library alpha 2 release

Postby qoda » Sun Feb 05, 2012 12:47 pm

I’ve been battling the entire weekend with the WiFly shield (Connected to a Arduino UNO). I know think I’ve exhausted all possible steps in debugging this issue. I have also tried this with all versions and some forks of the code and version 0022 and version 1.0 of the IDE.

After uploading and running SpiUartTerminal.pde or the HardwareFactoryReset.pde, the serial monitor just hangs after outputting “Waiting for input:” and doesn’t allow me to enter the command line application ($$$). I’ve tried unix screen, coolterm and the standard IDE serial monitor. I’ve also tested the pins to ensure everything is connected correctly (I finally soldered them to the header pins) and I’m sure it is.

I would really appreciate some help if possible. I’m now suspecting that it is in fact a hardware issue.
qoda
 
Posts: 3
Joined: Sun Feb 05, 2012 12:08 pm

Re: WiFly Shield code library alpha 2 release

Postby superbrudd » Fri Feb 17, 2012 5:07 pm

glibdud wrote:Are there any functions available that you can use to test that the WiFly is still associated with the WLAN? I poked through the source a bit, but didn't see anything obvious. I have it periodically checking a web page, and I'm guessing best practice is to check for association each time I go to hit it so that I can reconnect if necessary. Or does it just auto-reconnect if the connection drops? If so, can I trust that?

Thanks to the author for this library!


Did anyone find an answer to the above? At the moment, I'm setting my WiFly to reset every hour or so to avoid the 'random hang' issue - would be great to be able to detect when it has hung.

However the resetting is not working either... the WiFly library code seems to hang at the reboot stage. I've tried making it do hardware rebooting and software rebooting and neither work. I'm just sending data to pachube, not using it as a server, so I'm wondering whether anyone has an equivalent fix to the one that seems to work for the Server.cpp code?
superbrudd
 
Posts: 4
Joined: Sun Jul 24, 2005 9:58 pm

Re: WiFly Shield code library alpha 2 release

Postby misfit8d6 » Sat Feb 18, 2012 2:12 am

this library looks promising and it appears a major update isn't very far away... cheers!

http://arduinology.tumblr.com/
misfit8d6
 
Posts: 6
Joined: Wed Aug 06, 2008 7:45 am

PreviousNext

Return to Arduino

Who is online

Users browsing this forum: Google [Bot] and 2 guests