- Wed Sep 07, 2011 8:16 am
#133020
Hi everyone
I'm using the frontend SiGE GN3S sampler (ver. 2) on Ubuntu 10.10 (fresh install), and fx2-programmer to flash some firmware on the FE. After a few try, the frontend just disappear from lsusb, and I can't do anything with that since then. I also tried it on win 7 (which result in code 43) and win XP (which also failed), and couldn't even install the driver for it.
This is what happened:
1. I plugged in the FE in Ubuntu 10.10, run lsusb in terminal, it says my FE has VID=0x1781, PID=0x0b39, vendor name is "Multiple vendors"
2. I tried running make program with fx2-programmer:
3. I disconnect the module, then plugged in again. This time the module didn't show up on lsusb. No "multiple vendor", no 0x1781,... nothing, like it weren't even there.
I couldn't do anything to "talk" to the FE since then, as all I've got is the USB connection.
What should I do to make it normal again? Please help! Thank you all very much!
PS: I'm sorry for my bad English
I'm using the frontend SiGE GN3S sampler (ver. 2) on Ubuntu 10.10 (fresh install), and fx2-programmer to flash some firmware on the FE. After a few try, the frontend just disappear from lsusb, and I can't do anything with that since then. I also tried it on win 7 (which result in code 43) and win XP (which also failed), and couldn't even install the driver for it.
This is what happened:
1. I plugged in the FE in Ubuntu 10.10, run lsusb in terminal, it says my FE has VID=0x1781, PID=0x0b39, vendor name is "Multiple vendors"
2. I tried running make program with fx2-programmer:
Code: Select all
and it failed on the first command:
program:
./fx2-programmer $(VID) $(PID) set 0xE600 1
./fx2-programmer $(VID) $(PID) program $(FW_PATH)gn3s_firmware.ihx
./fx2-programmer $(VID) $(PID) set 0xE600 0
Code: Select all
I tried that command several times, with different VID and PID, and all failed. kazansky@kaz-ubuntu:~/GNSS/gn3s-linux/gn3s-linux/bin$ make program
./fx2-programmer 0x1781 0x0b39 set 0xE600 0
make: execvp: ./fx2-programmer: Permission denied
make: *** [program] Error 127
3. I disconnect the module, then plugged in again. This time the module didn't show up on lsusb. No "multiple vendor", no 0x1781,... nothing, like it weren't even there.
I couldn't do anything to "talk" to the FE since then, as all I've got is the USB connection.
What should I do to make it normal again? Please help! Thank you all very much!
PS: I'm sorry for my bad English