SparkFun Forums 

Where electronics enthusiasts find answers.

Have a good idea for a new product for SFE or Olimex? Let us know!
By noend
#112394
Everything you need to interface the TCM8230MD to a MCU is in the data sheet.
Last edited by noend on Tue Jan 04, 2011 10:15 am, edited 1 time in total.
By gentlemich
#113487
I am having a problem interfacing with the TCM8230MD on I2C using a Texas Instruments DM365 chip:

When reading the register (0x00 in this case) the I am getting the first Acknowledgement but not the second! Therefore nothing is happening and I cannot read the register.

I2c Read protocol: S SlaveAddress 0 A SubAddress A
Where SlaveAddress = 0x60 or 0x3c +0 and SubAddress = 0x00.

The first A (Acknowledgement) is OK but I am not sure if the second appears. Here are my screenshots:

Yellow = SDA; Blue=SCL
photo 1.JPG
You can see the yellow SDA line going down for the first Acknowledgement but there is no second A after sending the SubAddress.

Larger zoom (notice the long pause) :
3.jpg
My clock is at 10Mhz, my lines at 3VDC.

Any idea why?
You do not have the required permissions to view the files attached to this post.
By Roko
#113634
Do you mean your SCL Clock is at 10 MHz? If so perhaps try scaling it down a couple orders of magnitude. SCL Max is 400 khz according to general I2C specs, as well as the TCM8230 datasheet.

Edit: NM, if I'm reading your scope traces correctly you're more in the ballpark of 300-400 KHz, which should be fine.
By JustGreg
#113847
Hi everyone,

and greetings from me. I ordered two 8230 cams and I'll start experimenting as soon as they arrive. Anyway, has anyone tried the data transfer using an FTDI245 parallel FIFO USB chip? It has 8 data line can bedirectly connected to the camera DOUTs, and a 384 bytes FIFO. There would be no MCU action but to validate the lines at the FTDI's WR pin. Any idea?

@Dmitri

Would you be so kind as to name that battery pack on your picture? Thank you.
By Dmitri
#113917
JustGreg wrote:@Dmitri

Would you be so kind as to name that battery pack on your picture? Thank you.
It is something pleasantly cheap from China, bought at e***.com

70mAh
By gentlemich
#114120
gentlemich wrote: When reading the register (0x00 in this case) the I am getting the first Acknowledgement but not the second! Therefore nothing is happening and I cannot read the register.
I was able to solve the problem myself: the reason came from a poor soldering of the camera on the board...
I2C is ok and I even did not need any voltage translator (although the processor is at 3.3V the I2c line was limited at 3V by itself).
By snoop911
#115665
Can this (or any hobby camera) output raw (uncompressed) images?

My micro has limited space and a jpeg decoder doesn't fit.. I'd like to find a uart/spi camera that outputs 8-bits per pixel.. (@320x240 resolution would be nice). Even monochrome 1bpp would be fine!
By Dmitri
#116017
Hi all!

I'd like to make something clear. I cannot provide any assistance in building something similar nor I would sell a ready-to-use device.
The first is because my motivation for this has gone, the second is because of juristical reservations about unknown purpose.

The entire project is still on sale though.
By ohmeega
#116983
How do I use my webcam to remotely view my puppies from work? I have my webcam set up at home. When I get to work I would like to use it to view my puppies. At one time I had a free program I logged in to to do this but have lost it in a crash. Any ideas how I can do this?
______________________
affiliateelite ~ affiliateelite.com ~ adgooroo ~ adgooroo.com
Last edited by ohmeega on Sat Jan 15, 2011 12:57 am, edited 1 time in total.
  • 1
  • 24
  • 25
  • 26
  • 27
  • 28
  • 31