- Sun Nov 08, 2009 5:10 pm
#84610
UPDATE: Solved. Problem was a defective cable. Leaving my steps here in case anyone ever runs into a similar problem.
I have 2 MSP430-JTAG-TINY and 3 MSP430P1611, recently bought from sparkfun. I have reproduced the following problem under both WinXP and Win7.
First I downloaded the latest Olimex drivers (1.0.35) and the latest mspgcc (2008-12-30).
Then I installed mspgcc and copied the complete set of Olimex DLL files (5) to the mspgcc\bin folder. That should be it, right? I reboot, for Windows' sake. I always get this error:
After attempting to READ with the Olimex Programmer and closing the software, I get this error from msp430-jtag:
I have 2 MSP430-JTAG-TINY and 3 MSP430P1611, recently bought from sparkfun. I have reproduced the following problem under both WinXP and Win7.
First I downloaded the latest Olimex drivers (1.0.35) and the latest mspgcc (2008-12-30).
Then I installed mspgcc and copied the complete set of Olimex DLL files (5) to the mspgcc\bin folder. That should be it, right? I reboot, for Windows' sake. I always get this error:
Code: Select all
Now with the Olimex Programmer Software 1.21 I get equally bad results. Of course I updated its DLLs with the ones from the update previously listed. Then I run it, select MSP430F1611 from the list, USB port, then hit "read". It does something, because the LED turns off. But after a while, the program stops with "Cannot reseting device." (sic).C:\>msp430-jtag --lpt=USB
MSP430 JTAG programmer Version: 2.3
Use -h for help
Reset and release device...
An error occoured:
Could not reset target (no connection?): Could not communicate with FET
After attempting to READ with the Olimex Programmer and closing the software, I get this error from msp430-jtag:
Code: Select all
What am I doing wrong? The current driver is quite recent, has anyone else used it? I know I'm not TOO far because GDB seems to work. It identifies the device correctly.An error occoured:
Could not initialize the library (port: USB)
Code: Select all
C:\>msp430-gdbproxy --port=1000 msp430 USB
debug: MSP430_Initialize()
debug: MSP430_Configure()
debug: MSP430_VCC(3000)
debug: MSP430_Identify()
info: msp430: Target device is a 'MSP430F1611' (type 42)
debug: MSP430_Configure()
notice: msp430-gdbproxy: waiting on TCP port 1000
Last edited by denpanosekai on Sun Nov 15, 2009 8:55 am, edited 1 time in total.