MSP430F2013 Connect to serLCD

Discussions on how to get your MSP JTAG programmer up and running.

Moderator: phalanx

Post Reply
bjrosas
Posts: 2
Joined: Sun Jun 28, 2009 9:21 pm

MSP430F2013 Connect to serLCD

Post by bjrosas » Sun Jun 28, 2009 9:32 pm

Hello everyone, I am a newbie sorry if this is posted in the wrong forum. I just purchased a serLCD from sparkfun that says it can run off 3.3v source. I have a USB programmer that I have fed the two spy biwire connections and power to a breadboard to program a DIP MSP430. I am also powering the serLCD with this source and have a software implemented UART on my MSP430. I have set the DCO to 1MHZ and the and the timer_a to run at 9600 baud. When I supply power to the serLCD all I have is a screen with the backlight on, nothing is displayed. I try to send information through my software UART off of P1.0 and nothing happens. I currently have it configured for 8N1 communication does it need to be 1 start 8 data and 1 stop? Should jibberish be showing on the screen when I have it powered up? Am I not delivering enough power? Thanks!

naz
Posts: 108
Joined: Thu Feb 12, 2009 11:31 pm

Post by naz » Mon Jun 29, 2009 9:34 pm

why r u using software uart?.which microcontroller you are using?hardware uart is better than software uart.

User avatar
leon_heller
Support Volunteer
Posts: 5734
Joined: Sun May 01, 2005 11:20 am
Location: St. Leonards-on-Sea, E. Sussex, UK.

Post by leon_heller » Mon Jun 29, 2009 11:52 pm

Some MSP430s don't have a hardware UART! A software UART is very simple.

Leon
Leon Heller
G1HSM

bjrosas
Posts: 2
Joined: Sun Jun 28, 2009 9:21 pm

Post by bjrosas » Tue Jun 30, 2009 5:34 am

Okay, found out that my contrast pot was set too low. So for people who come across the same issue, on the back of the LCD seLCD backpack there is a small surface mount pot used to control the contrast. Thanks!

jimbobanderson
Posts: 1
Joined: Mon Jun 04, 2012 11:07 am

Re: MSP430F2013 Connect to serLCD

Post by jimbobanderson » Mon Jun 04, 2012 11:13 am

bjrosas - were you able to get this to work? I have been trying (and failing) to get my MSP430F2013 to do a serial communication at 9600 baud for months. Any insights/code you could share would be GREATLY appreciated.

Post Reply