- Thu Jun 18, 2009 11:20 am
#75267
Hi,
I am new with the MSP430 stuff.
I have a eZ430-RF2500 kit and I was planning to use it as a Flash Emulation Tool. Just make sure, I connected the MSP430 that comes with the kit (MSP430F2274) and tried to debug using IAR 4.0 version. But appeared this error:
Wed Jun 17 20:49:53 2009: Fatal error: Failed to initialize.
Check if hardware connected.
Check if drivers are installed.
Try to restart the computer.
Tools using the parallel port are not supported on Windows Vista
Session aborted!
Wed Jun 17 20:49:58 2009: Failed to load debugee: C:\MSP430\Release\Exe\TC2009.txt
The code is this:
#include "msp430x22x4.h"
OBS: The hardware was connected and installed and I am using Windows XP.
Please, I tried everything but didn't help. Anyone else knows why?
I am new with the MSP430 stuff.
I have a eZ430-RF2500 kit and I was planning to use it as a Flash Emulation Tool. Just make sure, I connected the MSP430 that comes with the kit (MSP430F2274) and tried to debug using IAR 4.0 version. But appeared this error:
Wed Jun 17 20:49:53 2009: Fatal error: Failed to initialize.
Check if hardware connected.
Check if drivers are installed.
Try to restart the computer.
Tools using the parallel port are not supported on Windows Vista
Session aborted!
Wed Jun 17 20:49:58 2009: Failed to load debugee: C:\MSP430\Release\Exe\TC2009.txt
The code is this:
#include "msp430x22x4.h"
Code: Select all
int main( void )
{
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;
P1DIR = 1;
while (1);
{
}
}
OBS: The hardware was connected and installed and I am using Windows XP.
Please, I tried everything but didn't help. Anyone else knows why?