- Thu Jun 04, 2009 4:32 pm
#74200
Hello, I'm a BSEE student working on a senior design project. I'm using the MSP430f2013 and I'm trying to program a LCD display. Eventually I'd like to use the MSP430 to display battery voltage using the ADC, but first I have to get the LCD to work. All it does right now is show all black boxes. I have some code but it's not working and I'm hoping someone may be able to steer me in the right direction. I don't have much experience programming micro-controllers by the way..
#include "io430.h"
#include "intrinsics.h"
#define DB4 BIT3
#define DB5 BIT2
#define DB6 BIT1
#define DB7 BIT0
#define E BIT4
#define RS BIT5
void wait(int ms); // wait for some designated milliseconds
void initialize_LCD(); // execute all the preferences, setup & initialization commands on the LCD
void send_LCD(int data, int rs_flag); // sends word to LCD and sets rs flag
void print_LCD(char* msg); // sends a specified string to the LCD, also clears the screen
void LCD_cmd(int command); // execute a specific command on the LCD. Sets flag correctly.
void LCD_data(char charcode); // send one character to the LCD, without clearing the screen first. Sets flag correctly.
int main( void )
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer to prevent time out reset
P1DIR = RS | E | DB7 | DB6 | DB5 | DB4; //Set the data, RS & E pins to output
P1OUT = 0; //Initialize output to zero/low.
initialize_LCD(); //Send our preferences to the LCD and initialize.
print_LCD("Testing");
__low_power_mode_4(); // Execution doesn't won't move past this line.
return 0;
}
//Set up LCD preferences and initiate initialization commands
void initialize_LCD()
{
wait(50); //Wait a little bit for the LCD to reach supply voltage.
//Set to 4-bit mode
P1OUT &= ~(RS); //this is a command, not data
wait(5);
send_LCD(0x02, 0);
wait(20);
LCD_cmd(0x28); // set 4bitmode: 1-Line Mode and 5x8 Font
wait(20);
LCD_cmd(0x0F); // Main Screen Turn On (Display ON) Use a cursor that blinks.
wait(20);
LCD_cmd(0x06); // Move the cursor from left to right on a character entry.
wait(20);
LCD_cmd(0x01); // Clear Display. Also resets the cursor to the first char on the left.
wait(20);
}
//Wait a designated amount of time in milliseconds.
void wait(int ms)
{
int whileCount = 0;
TACTL = MC_1 | ID_2 | TASSEL_2 | TACLR;
TACCR0 = 274;
for(int i=0; i<ms; i++)
{
while(TACTL_bit.TAIFG == 0) {
whileCount++;
}
TACTL_bit.TAIFG = 0;
}
}
// Send one word of data to the LCD, then clock it.
void send_LCD(int data, int rs_flag)
{
P1OUT |= E; // LCD Clocked High
P1OUT |= (data | 0xF); //Load up the data
if(rs_flag) { P1OUT |= RS; } //If RS is high, make sure it sends as 1.
else { P1OUT &= ~(RS); } //otherwise, specifically disable it.
wait(10);
P1OUT &= ~(E); // E low, activate LCD.
wait(10);
P1OUT &= ~(DB4 | DB5 | DB6 | DB7); //clear the data bits
}
//send a character code to the LCD:
void LCD_data(char charcode)
{
send_LCD( ((charcode&0xF0) >> 4), 1 ); //High nibble is sent first (4bit mode) RS=1
wait(20);
send_LCD( ((charcode&0x0F)), 1 ); //Followed by the low nibble (4bit mode) RS=1
wait(20);
}
//send a command to the LCD:
void LCD_cmd(int command)
{
wait(20);
send_LCD( ((command&0xF0) >> 4), 0 ); //High nibble is sent first (4bit mode) RS = 0
wait(20);
send_LCD( (command&0x0F), 0 ); //Followed by the low nibble (4bit mode) RS = 0
wait(20);
}
// Print out a full string to the LCD
void print_LCD(char* msg)
{
LCD_cmd(0x01); //clear the LCD
wait(20);
while (*msg) {
LCD_data(*msg);
msg++;
}
}
#include "io430.h"
#include "intrinsics.h"
#define DB4 BIT3
#define DB5 BIT2
#define DB6 BIT1
#define DB7 BIT0
#define E BIT4
#define RS BIT5
void wait(int ms); // wait for some designated milliseconds
void initialize_LCD(); // execute all the preferences, setup & initialization commands on the LCD
void send_LCD(int data, int rs_flag); // sends word to LCD and sets rs flag
void print_LCD(char* msg); // sends a specified string to the LCD, also clears the screen
void LCD_cmd(int command); // execute a specific command on the LCD. Sets flag correctly.
void LCD_data(char charcode); // send one character to the LCD, without clearing the screen first. Sets flag correctly.
int main( void )
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer to prevent time out reset
P1DIR = RS | E | DB7 | DB6 | DB5 | DB4; //Set the data, RS & E pins to output
P1OUT = 0; //Initialize output to zero/low.
initialize_LCD(); //Send our preferences to the LCD and initialize.
print_LCD("Testing");
__low_power_mode_4(); // Execution doesn't won't move past this line.
return 0;
}
//Set up LCD preferences and initiate initialization commands
void initialize_LCD()
{
wait(50); //Wait a little bit for the LCD to reach supply voltage.
//Set to 4-bit mode
P1OUT &= ~(RS); //this is a command, not data
wait(5);
send_LCD(0x02, 0);
wait(20);
LCD_cmd(0x28); // set 4bitmode: 1-Line Mode and 5x8 Font
wait(20);
LCD_cmd(0x0F); // Main Screen Turn On (Display ON) Use a cursor that blinks.
wait(20);
LCD_cmd(0x06); // Move the cursor from left to right on a character entry.
wait(20);
LCD_cmd(0x01); // Clear Display. Also resets the cursor to the first char on the left.
wait(20);
}
//Wait a designated amount of time in milliseconds.
void wait(int ms)
{
int whileCount = 0;
TACTL = MC_1 | ID_2 | TASSEL_2 | TACLR;
TACCR0 = 274;
for(int i=0; i<ms; i++)
{
while(TACTL_bit.TAIFG == 0) {
whileCount++;
}
TACTL_bit.TAIFG = 0;
}
}
// Send one word of data to the LCD, then clock it.
void send_LCD(int data, int rs_flag)
{
P1OUT |= E; // LCD Clocked High
P1OUT |= (data | 0xF); //Load up the data
if(rs_flag) { P1OUT |= RS; } //If RS is high, make sure it sends as 1.
else { P1OUT &= ~(RS); } //otherwise, specifically disable it.
wait(10);
P1OUT &= ~(E); // E low, activate LCD.
wait(10);
P1OUT &= ~(DB4 | DB5 | DB6 | DB7); //clear the data bits
}
//send a character code to the LCD:
void LCD_data(char charcode)
{
send_LCD( ((charcode&0xF0) >> 4), 1 ); //High nibble is sent first (4bit mode) RS=1
wait(20);
send_LCD( ((charcode&0x0F)), 1 ); //Followed by the low nibble (4bit mode) RS=1
wait(20);
}
//send a command to the LCD:
void LCD_cmd(int command)
{
wait(20);
send_LCD( ((command&0xF0) >> 4), 0 ); //High nibble is sent first (4bit mode) RS = 0
wait(20);
send_LCD( (command&0x0F), 0 ); //Followed by the low nibble (4bit mode) RS = 0
wait(20);
}
// Print out a full string to the LCD
void print_LCD(char* msg)
{
LCD_cmd(0x01); //clear the LCD
wait(20);
while (*msg) {
LCD_data(*msg);
msg++;
}
}