- Wed Aug 24, 2005 2:59 pm
#6718
Is anyone knows why when iam debugging my code:void Init8900(void)
{
unsigned int i;
P3OUT = IOR | IOW; // reset outputs, control lines high
P3DIR = 0xff; // switch control port to output
P5OUT = 0; // reset outputs
P5DIR = 0xff; // switch data port to output
DelayCycles(40000); // delay 10ms @ 8MHz MCLK to allow
DelayCycles(40000); // time for CS8900 POR
Write8900(ADD_PORT, PP_SelfCTL); // set register
Write8900(DATA_PORT, POWER_ON_RESET); // reset the Ethernet-Controller
do
Write8900(ADD_PORT, PP_SelfST); // set register
while (!(Read8900(DATA_PORT) & INIT_DONE)); // wait until chip-reset is done
for (i = 0; i < sizeof InitSeq / sizeof (TInitSeq); i++) // configure the CS8900
{
Write8900(ADD_PORT, InitSeq.Addr);
Write8900(DATA_PORT, InitSeq.Data);
}
}
never lives from that lop.When i connect my board whith my pc will it works?[/code]
{
unsigned int i;
P3OUT = IOR | IOW; // reset outputs, control lines high
P3DIR = 0xff; // switch control port to output
P5OUT = 0; // reset outputs
P5DIR = 0xff; // switch data port to output
DelayCycles(40000); // delay 10ms @ 8MHz MCLK to allow
DelayCycles(40000); // time for CS8900 POR
Write8900(ADD_PORT, PP_SelfCTL); // set register
Write8900(DATA_PORT, POWER_ON_RESET); // reset the Ethernet-Controller
do
Write8900(ADD_PORT, PP_SelfST); // set register
while (!(Read8900(DATA_PORT) & INIT_DONE)); // wait until chip-reset is done
for (i = 0; i < sizeof InitSeq / sizeof (TInitSeq); i++) // configure the CS8900
{
Write8900(ADD_PORT, InitSeq.Addr);
Write8900(DATA_PORT, InitSeq.Data);
}
}
never lives from that lop.When i connect my board whith my pc will it works?[/code]