- Mon Jul 14, 2008 11:53 am
#51852
#include "LCD.h"
#include "msp430xG46x.h"
#include "stdio.h"
/*
#define SEG_A 0x01
#define SEG_B 0x02
#define SEG_C 0x04
#define SEG_D 0x08
#define SEG_E 0x40
#define SEG_F 0x10
#define SEG_G 0x20
#define SEG_H 0x80
*/
const int charseg[]=
{
LCD_A+LCD_B+LCD_C+LCD_D+LCD_E+LCD_F, // '0' or 'O'
LCD_B+LCD_C, // '1' or 'I'
LCD_A+LCD_B+LCD_D+LCD_E+LCD_G, // '2' or 'Z'
LCD_A+LCD_B+LCD_C+LCD_D+LCD_G, // '3'
LCD_B+LCD_C+LCD_F+LCD_G, // '4' or 'y'
LCD_A+LCD_C+LCD_D+LCD_F+LCD_G, // '5' or 'S'
LCD_A+LCD_C+LCD_D+LCD_E+LCD_F+LCD_G, // '6' or 'b'
LCD_A+LCD_B+LCD_C, // '7'
LCD_A+LCD_B+LCD_C+LCD_D+LCD_E+LCD_F+LCD_G, // '8' or 'B'
LCD_A+LCD_B+LCD_C+LCD_F+LCD_G // '9' or 'g'
};
void disp(double num)
{
if(num>18888888)
{
LCDM7=LCD_A+LCD_D+LCD_E+LCD_F+LCD_G;
LCDM6=LCD_E+LCD_G;
LCDM5=LCD_E+LCD_G;
}
else if(num>9999999)
{
LCDMEM[12]|=LCD_D;
}
printf("%.1f", num);
}
void main(void)
{
int i,pos=0,index;
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
FLL_CTL0 |= XCAP14PF; // Configure load caps
P5SEL = 0x1C; // P5.2/3/4 = LCD COM lines
for (i = 19; i > 0; i--) LCDMEM = 0; // Clear LCD
LCDACTL = LCDON + LCD4MUX + LCDFREQ_128; // 4mux LCD, ACLK/128
LCDAPCTL0 = 0x7E; // Segments 4-27
disp(18888890);
}
this is my code under development but m getting
Fatal Error[e89]: Too much object code produced (more than 0x1000 bytes) for this package
this error what do i do please help me