SparkFun Forums 

Where electronics enthusiasts find answers.

Questions &/or issues related to products in the Kits category should be posted in this forum.
#207639
Hi. I purchased LCD-10862 for use with the Variable Load kit. I noticed that on the standard "basic" one color 16 pin LCD,
that pin 15 is A +4.2 V and pin 16 is K (0V).

However, on the RGB LCD-10862 pinout, it lists pin 15 as K and pin 16 as A-RED (opposite of "basic" LCD.

What is the correct way to connect LCD-10862 to the load board? Do I need to swap pins 15/16 for to connect it correctly?

Thanks!
Jaime
#207670
Hi Jamie,

Pins 15 and 16 on the Variable Load Kit are actually not connected to anything so powering the backlight for the RGB LCD will require running a couple of wires to use one of the colors. The easiest option would be to run a power and ground wire to the 5V and Ground pins on the side of the Load Kit mainboard like this (assuming you want to use the Red LED for your backlight):
green_wire_fix.jpg
Excuse the MS paint and bad coloring (just to clarify, green=Vcc/5V and black=Ground) and just make sure to add a 330ohm resistor in series with the power line for your Red LED and that should work to power the backlight. If you wanted to use the other colors, you would just run the wire from 5V to whichever color LED you want along with that 330ohm resistor to limit the current.

I hope this helps you hook up your RGB LCD with the Variable Load Kit. Let us know if you have any other questions or concerns about using these products and we would be happy to help as much as we can.
You do not have the required permissions to view the files attached to this post.
#207746
Hi again. One more thing if you don't mind.

Is the "LOAD ON" LED supposed to REMAIN on after pressing enter? or just flash green quickly and turn back off? The Hookup Guide says " The "Enter" key turns the load on or off ..." but I'm unsure what state the LED should show if it is working.

Thanks!
Jaime
#207828
Hmm, I am not sure what would be going on there at the moment. If you open a serial terminal to control the kit, do you get normal behavior as described in this section of the Hookup Guide? Also, can you take a few photos of the top and bottom of your kit and attach them to your reply? Please do your best to make sure they are clear and well-lit.
#207944
Hi Jamie,

You should be able to attach photos using the "Reply" button or clicking the "Full Editor & Preview" when you open the Quick Reply option and then underneath the "text box" select "Upload Attachment". You can either put them inline or just leave them at the end. Alternatively, you can host them on something like Google Drive and link them in your reply. I use this page for instructions on adding images and a whole host of other formatting options for the software our forums run on.
#207946
Hmm, if you cannot upload the photos and your NW admin cannot work it out, you may just need to host them somewhere else and link it. If that won't work, send me a PM and we can work something out to get the photos up.
#207981
Hi again Jamie,

I was able to take a look at your photos and nothing stands out in the hardware that would be causing this problem. Does the kit behave normally either displaying to the display or to a serial terminal aside from the LOAD LED? If not, did you by chance test the kit prior to attaching the LCD? Did it function normally then?
#207984
Hi Mark.

Okay, thanks for taking a look. I did not test it prior to installing the LCD. I will play with it some more and see if there is something I am missing here. Then if it doesn't work out, I can try to remove the LCD and see if it changes anything.

Thanks for you help!
Jaime
#208012
The display really should not affect the functionality of the firmware so I would leave removing the LCD as a last-ditch effort unless you have the right tools for desoldering PTH components. Try testing via serial terminal and with the display to see if you can get the Load Kit working as expected.