- Fri Feb 29, 2008 11:30 pm
#43810
Hi all,
So I'm making some headway learning about this DX160.
Everything seems to be working. But when I send a second update to the screen - it just blanks out and seems to die. Not sure if this is my code or what.
It also does then when I try to change my font size. Argh, I wish there was more documentation :)
Any help would be greatly appreciated!
So I'm making some headway learning about this DX160.
Everything seems to be working. But when I send a second update to the screen - it just blanks out and seems to die. Not sure if this is my code or what.
It also does then when I try to change my font size. Argh, I wish there was more documentation :)
Any help would be greatly appreciated!
Code: Select all
char incomingByte; // Serial communication
char tmpOutput[200]; // Store incoming serial communication
char *cursor;
char *str = "";
int count = 0;
int speaker = 9;
int led = 13;
int btn = 10;
void setup() {
pinMode(speaker, OUTPUT);
pinMode(led, OUTPUT);
Serial.begin(57600);
digitalWrite(led, HIGH);
}
void loop() {
if (Serial.available() > 0) {
if (incomingByte != 13) {
incomingByte = Serial.read();
tmpOutput[count] = incomingByte;
count++;
}
if (incomingByte == 13) {
clearDisplay();
say(tmpOutput);
Serial.print(255, BYTE);delay(10);
count=0;
delay(2000);
}
}
}
void clearDisplay() {
Serial.print(186, BYTE);
delay(100);
}
void say(char* text) {
for(cursor=text; *cursor != '\0'; ++cursor) {
Serial.print(*cursor, BYTE);
}
}
void setSmallFont() {
Serial.print(181, BYTE);
delay(10);
}
void setLargeFont() {
Serial.print(180, BYTE);
delay(10);
}