- Wed Feb 14, 2007 8:44 pm
#26153
HI!
I am having some problems with my code for the trf24g and find it cind of difficult to debug internaly in the reciver. The sender sends one byte of data into the tranciver, but the DR1 pin on the reciver doesent go high at any time.
I would apriciate any help i can get.
RX code :
TX code:
I am having some problems with my code for the trf24g and find it cind of difficult to debug internaly in the reciver. The sender sends one byte of data into the tranciver, but the DR1 pin on the reciver doesent go high at any time.
I would apriciate any help i can get.
RX code :
Code: Select all
#include <mega16.h>
#include <stdio.h>
#include <delay.h>
#define CE PORTB.0
#define CS PORTB.1
//*******************************************************************************************
// configuration word : (15 bytes)
/*15*/ #define TRF24G_PAYLOAD_SIZE_1 1 // in bytes
/*14*/ #define TRF24G_PAYLOAD_SIZE_2 1 // in bytes
/*9-13*/ #define TRF24G_ADDR_2 0,0,0,0,0 // 5 bytes (not in use)
/*4-8*/ #define TRF24G_ADDR_1 0,0,0,0,0xAA // 5 bytes
/*3*/ #define TRF24G_ADDR_SIZE 1 // in bytes
#define TRF24G_CRC_SIZE 0b01 // 8 bit CRC enabled
/*2*/ #define TRF24G_RX2_EN 0 // RX2 dissabled
#define TRF24G_SHOCK_EN 1 // shock burst enabled
#define TRF24G_DATARATE 0 // 0 for 250kbs or 1 for 1mbs
#define TRF24G_XTAL_FREQ 0b011 // 16mhz inside unit
#define TRF24G_TX_PWR 0b11 // FULL power !!
/*1*/ #define TRF24G_CHANNEL 2 // channel 2
#define TRF24G_RX 0 // 0 for TX or 1 for RX
// end of config word.
//******************************************************************************************
// tabell for configurerings ordet.
static unsigned char trf24gConfig[15] = {
/*15*/ TRF24G_PAYLOAD_SIZE_2 * 8, // DATA2_W in bits
/*14*/ TRF24G_PAYLOAD_SIZE_1 * 8, // DATA1_W in bits
/*9-13*/ TRF24G_ADDR_2, // ADDR2 (not in use)
/*4-8*/ TRF24G_ADDR_1, // ADDR1
/*3*/ ((TRF24G_ADDR_SIZE * 8) << 2) | TRF24G_CRC_SIZE,
/*2*/ (TRF24G_RX2_EN << 7) | // RX2 active?
(TRF24G_SHOCK_EN << 6) | // Shockburst?
(TRF24G_DATARATE << 5) | // Datarate
(TRF24G_XTAL_FREQ << 2) | // xtal frequency
TRF24G_TX_PWR , // Tx power
/*1*/ (TRF24G_CHANNEL << 1) | TRF24G_RX // Channel and RX/TX select
};
//***************************************************************************************
void vent ()
{
delay_ms(5);
}
//*********************************************************************************
void spiSend(unsigned char data)
{
#asm("cli") // disable interrupts
SPDR = data;
while(SPSR == 0x00)
{
//wait for sending to finish
}
#asm("sei") // enable interrupts
}
//****************************************************************************************
void trf24gconfigure(unsigned char trf24gConfig[15]) {
unsigned char i;
delay_ms(3); // 3ms startup
CE = 0 ;
vent() ; // enter config mode
CS = 1 ;
for(i = 0; i < sizeof(trf24gConfig); i++)
{
spiSend(trf24gConfig[i]); // sending...
}
CS = 0 ; // exit config mode
vent() ;
#if TRF24G_RX
CE = 1 ; // activate RX
vent() ;
#endif
}
//****************** RECIVING ***********************************************************
// External Interrupt 0 service routine (interupts when data ready (DR =1) )
interrupt [EXT_INT0] void ext_int0_isr(void)
{
unsigned char data;
int i ;
unsigned char size = TRF24G_PAYLOAD_SIZE_1;
printf ("\n\r%d", 0x22 ) ; // for debug
#asm("cli") // disable interupt
printf ("\n\r%d", 0x21 ) ; // for debug
spiSend (0x00) ; // sends 0, when finished SPI interrupts
for(i = 0; i < size ; i++)
{
data = SPDR ;
printf ("\n\r%d", 0x20 ) ; // for debug
printf ("\n\r%d", data ) ;
spiSend (0x00) ;
}
vent() ;
#asm("sei") // enable interupt
}
//*****************************************************************************************************
void main(void)
{
PORTB=0x00;
DDRB=0xB3;
PORTD=0x00;
DDRD=0x02;
// SPI initialization
// SPI Type: Master
// SPI Clock Rate: 62,000 kHz
// SPI Clock Phase: Cycle Half
// SPI Clock Polarity: Low
// SPI Data Order: MSB First
SPCR=0x53;
SPSR=0x00;
//USART
UCSRA=0x00;
UCSRB=0x18;
UCSRC=0x86;
UBRRH=0x00;
UBRRL=0x33;
// External Interrupt(s) initialization
// INT0: On
// INT0 Mode: Rising Edge
// INT1: Off
// INT2: Off
GICR|=0x40;
MCUCR=0x03;
MCUCSR=0x00;
GIFR=0x40;
// Clear the SPI interrupt flag
#asm
in r30,spsr
in r30,spdr
#endasm
// Global enable interrupts
#asm("sei")
trf24gconfigure(trf24gConfig); // configure RF24g
while (1)
{
//just let the interupt work(RX-mode)
}
}// main
TX code:
Code: Select all
// transmitter code for RF 24g
#include <mega8.h>
#include <stdio.h>
#include <delay.h>
#define CE PORTB.6
#define CS PORTB.7
//*******************************************************************************************
// configuration word : (15 bytes)
/*15*/ #define TRF24G_PAYLOAD_SIZE_1 1 // in bytes
/*14*/ #define TRF24G_PAYLOAD_SIZE_2 1 // in bytes
/*9-13*/ #define TRF24G_ADDR_2 0,0,0,0,0 // 5 bytes (not in use)
/*4-8*/ #define TRF24G_ADDR_1 0,0,0,0,0xAA // 5 bytes
/*3*/ #define TRF24G_ADDR_SIZE 1 // in bytes
#define TRF24G_CRC_SIZE 0b01 // 8 bit CRC enabled
/*2*/ #define TRF24G_RX2_EN 0 // RX2 dissabled
#define TRF24G_SHOCK_EN 1 // shock burst enabled
#define TRF24G_DATARATE 0 // 0 for 250kbs or 1 for 1mbs
#define TRF24G_XTAL_FREQ 0b011 // 16mhz inside unit
#define TRF24G_RX_PWR 0b11 // FULL power !!
/*1*/ #define TRF24G_CHANNEL 2 // channel 2
#define TRF24G_RX 0 // 0 for TX or 1 for RX
// end of config word.
//******************************************************************************************
unsigned char trf24gConfig[15] = { // tabell for configurerings ordet.
/*15*/ TRF24G_PAYLOAD_SIZE_2 * 8, // DATA2_W in bits
/*14*/ TRF24G_PAYLOAD_SIZE_1 * 8, // DATA1_W in bits
/*9-13*/ TRF24G_ADDR_2, // ADDR2 (not in use)
/*4-8*/ TRF24G_ADDR_1, // ADDR1
/*3*/ ((TRF24G_ADDR_SIZE * 8) << 2) | TRF24G_CRC_SIZE,
/*2*/ (TRF24G_RX2_EN << 7) | // RX2 active?
(TRF24G_SHOCK_EN << 6) | // Shockburst?
(TRF24G_DATARATE << 5) | // Datarate
(TRF24G_XTAL_FREQ << 2) | // xtal frequency
TRF24G_RX_PWR , // Tx power
/*1*/ (TRF24G_CHANNEL << 1) | TRF24G_RX // Channel and RX/TX select
};
//***************************************************************************************
void vent ()
{
delay_us(5);
}
//*********************************************************************************
void spiSend(unsigned char data)
{
SPDR = data;
while(SPSR == 0x00)
{
//wait for sending to finish
}
}
//****************************************************************************************
void trf24gconfigure(unsigned char trf24gConfig[15])
{
unsigned char i;
delay_ms(3); // 3ms startup
CE = 0 ;
vent() ; // enter config mode
CS = 1 ;
for(i = 0; i < sizeof(trf24gConfig); i++)
{
spiSend(trf24gConfig[i]); // sending...
}
CS = 0 ; // exit config mode
vent() ;
#if TRF24G_RX
CE = 1 ; // activate RX
#endif
}
//******************************************************************************************
void trf24gSend(char data) // for 1 byte data and address
{
unsigned char addr = 0xAA;
CE = 1 ;
vent() ; // enter sending mode
CS = 0 ;
spiSend(addr); //adress
vent () ;
spiSend(data); // DATA
vent () ;
CE = 0 ; //back to standby
}
//*****************************************************************************************************
void main(void)
{
PORTB=0x00;
DDRB=0xFF;
PORTC=0x00;
DDRC=0x00;
// SPI initialization
// SPI Type: Master
// SPI Clock Rate: 62,000 kHz
// SPI Clock Phase: Cycle Half
// SPI Clock Polarity: Low
// SPI Data Order: MSB First
SPCR=0x53;
SPSR=0x00;
//USART
UCSRA=0x00;
UCSRB=0x18;
UCSRC=0x86;
UBRRH=0x00;
UBRRL=0x33;
trf24gconfigure(trf24gConfig); // configure RF24g
while (1)
{
trf24gSend(0x24) ;
delay_ms (1000) ;
}
}// main
Sigve
Everything flies, you just need a big enougth engine :D
Everything flies, you just need a big enougth engine :D