- Sun Sep 16, 2007 11:45 am
#35177
So i was going through the embedded electronics tutorial and i was wondering how to change the code in the tutorial 2 to work for an attiny13
here is the source:
here is the source:
Code: Select all
thanks/*
5-10-07
Copyright Spark Fun Electronics© 2007
Nathan Seidle
nathan at sparkfun.com
Example Blink
Toggles all IO pins at 1Hz
*/
#include <avr/io.h>
//Define functions
//======================
void ioinit(void); //Initializes IO
void delay_ms(uint16_t x); //General purpose delay
//======================
int main (void)
{
ioinit(); //Setup IO pins and defaults
while(1)
{
PORTC = 0xFF;
PORTB = 0xFF;
PORTD = 0xFF;
delay_ms(500);
PORTC = 0x00;
PORTB = 0x00;
PORTD = 0x00;
delay_ms(500);
}
return(0);
}
void ioinit (void)
{
//1 = output, 0 = input
DDRB = 0b11111111; //All outputs
DDRC = 0b11111111; //All outputs
DDRD = 0b11111110; //PORTD (RX on PD0)
}
//General short delays
void delay_ms(uint16_t x)
{
uint8_t y, z;
for ( ; x > 0 ; x--){
for ( y = 0 ; y < 90 ; y++){
for ( z = 0 ; z < 6 ; z++){
asm volatile ("nop");
}
}
}
}