- Wed Aug 29, 2007 1:02 am
#34414
Hi,
i'm trying at the moment to execute a simple interrupt through a Button (Button2) while a LED is blinking, but nothing happens!
I've got the EK Boad from Olimex.
The button is connected with PA20 which is also IRQ0.
Would be great is someone have 2-3 minutes to have a look on m code, thanks!
Regards from cologne!
Tobi
main.c:
--------------------------------------------------
#include "AT91SAM7S256.h"
#include "board.h"
#include "delay.h"
#include "stdlib.h"
#include "string.h"
void button2irqhandler (void);
extern void LowLevelInit(void);
extern unsigned enableIRQ(void);
void LowLevelInit();
int main (void) {
// Set up the LEDs (PA0 - PA3)
volatile AT91PS_PIO pPIO = AT91C_BASE_PIOA; // pointer to PIO
data structure
pPIO->PIO_PER = LED_MASK | Button2; // PIO Enable Register -
allow PIO to control pins P0 - P2 and pin 19
pPIO->PIO_OER = LED_MASK; // PIO Output Enable Register -
sets pins P0 - P2 to outputs
pPIO->PIO_SODR = LED_MASK; // PIO Set Output Data
Register - turns off the two LEDs
// Select PA20 (pushbutton) to be IRQ function (Peripheral B)
pPIO->PIO_BSR = Button2;
// Set up the AIC registers for Button2
volatile AT91PS_AIC pAIC = AT91C_BASE_AIC; // pointer to AIC
data structure
pAIC->AIC_IDCR = (1<<AT91C_ID_IRQ0); // Disable IRQ0 interrupt
in AIC Interrupt Disable Command Register
pAIC->AIC_SVR[AT91C_ID_IRQ0] = // Set the Button2 IRQ0
handler address in AIC Source
(unsigned int)button2irqhandler; // Vector Register[30]
pAIC->AIC_SMR[AT91C_ID_IRQ0] = // Set the interrupt source
type and priority
(AT91C_AIC_SRCTYPE_INT_HIGH_LEVEL | 0x4 ); // in AIC Source Mode
Register[30]
pAIC->AIC_ICCR = (1<<AT91C_ID_IRQ0); // Clear the IRQ0
interrupt in AIC Interrupt Clear Command Register
pAIC->AIC_IDCR = (0<<AT91C_ID_IRQ0); // Remove disable IRQ0
interrupt in AIC Interrupt Disable Command Reg
pAIC->AIC_IECR = (1<<AT91C_ID_IRQ0); // Enable the IRQ0
interrupt in AIC Interrupt Enable Command Register
enableIRQ();
while (1) {
Delay(500);
if ((pPIO->PIO_ODSR & LED1) == LED1) { // read previous state
of LED1
pPIO->PIO_CODR = LED1;
} else {
pPIO->PIO_SODR = LED1;
}
}
}
---------------------------------------------
button2isr.c:
---------------------------------------------
#include "AT91SAM7S256.h"
#include "board.h"
void button2irqhandler (void) {
volatile AT91PS_TC pTC = AT91C_BASE_TC0; // pointer to timer
channel 0 register structure
volatile AT91PS_PIO pPIO = AT91C_BASE_PIOA; // pointer to PIO
register structure
unsigned int dummy; // temporary
dummy = pTC->TC_SR; // read TC0 Status Register to
clear interrupt
if ((pPIO->PIO_ODSR & LED2) == LED2) {
pPIO->PIO_CODR = LED2; // turn LED2 (DS2) on
} else {
pPIO->PIO_SODR = LED2; // turn LED2 (DS2) off
}
}
------------------------------------------
unsigned enableIRQ(void)
{
unsigned _cpsr;
_cpsr = __get_cpsr();
__set_cpsr(_cpsr & ~IRQ_MASK);
return _cpsr;
}
i'm trying at the moment to execute a simple interrupt through a Button (Button2) while a LED is blinking, but nothing happens!
I've got the EK Boad from Olimex.
The button is connected with PA20 which is also IRQ0.
Would be great is someone have 2-3 minutes to have a look on m code, thanks!
Regards from cologne!
Tobi
main.c:
--------------------------------------------------
#include "AT91SAM7S256.h"
#include "board.h"
#include "delay.h"
#include "stdlib.h"
#include "string.h"
void button2irqhandler (void);
extern void LowLevelInit(void);
extern unsigned enableIRQ(void);
void LowLevelInit();
int main (void) {
// Set up the LEDs (PA0 - PA3)
volatile AT91PS_PIO pPIO = AT91C_BASE_PIOA; // pointer to PIO
data structure
pPIO->PIO_PER = LED_MASK | Button2; // PIO Enable Register -
allow PIO to control pins P0 - P2 and pin 19
pPIO->PIO_OER = LED_MASK; // PIO Output Enable Register -
sets pins P0 - P2 to outputs
pPIO->PIO_SODR = LED_MASK; // PIO Set Output Data
Register - turns off the two LEDs
// Select PA20 (pushbutton) to be IRQ function (Peripheral B)
pPIO->PIO_BSR = Button2;
// Set up the AIC registers for Button2
volatile AT91PS_AIC pAIC = AT91C_BASE_AIC; // pointer to AIC
data structure
pAIC->AIC_IDCR = (1<<AT91C_ID_IRQ0); // Disable IRQ0 interrupt
in AIC Interrupt Disable Command Register
pAIC->AIC_SVR[AT91C_ID_IRQ0] = // Set the Button2 IRQ0
handler address in AIC Source
(unsigned int)button2irqhandler; // Vector Register[30]
pAIC->AIC_SMR[AT91C_ID_IRQ0] = // Set the interrupt source
type and priority
(AT91C_AIC_SRCTYPE_INT_HIGH_LEVEL | 0x4 ); // in AIC Source Mode
Register[30]
pAIC->AIC_ICCR = (1<<AT91C_ID_IRQ0); // Clear the IRQ0
interrupt in AIC Interrupt Clear Command Register
pAIC->AIC_IDCR = (0<<AT91C_ID_IRQ0); // Remove disable IRQ0
interrupt in AIC Interrupt Disable Command Reg
pAIC->AIC_IECR = (1<<AT91C_ID_IRQ0); // Enable the IRQ0
interrupt in AIC Interrupt Enable Command Register
enableIRQ();
while (1) {
Delay(500);
if ((pPIO->PIO_ODSR & LED1) == LED1) { // read previous state
of LED1
pPIO->PIO_CODR = LED1;
} else {
pPIO->PIO_SODR = LED1;
}
}
}
---------------------------------------------
button2isr.c:
---------------------------------------------
#include "AT91SAM7S256.h"
#include "board.h"
void button2irqhandler (void) {
volatile AT91PS_TC pTC = AT91C_BASE_TC0; // pointer to timer
channel 0 register structure
volatile AT91PS_PIO pPIO = AT91C_BASE_PIOA; // pointer to PIO
register structure
unsigned int dummy; // temporary
dummy = pTC->TC_SR; // read TC0 Status Register to
clear interrupt
if ((pPIO->PIO_ODSR & LED2) == LED2) {
pPIO->PIO_CODR = LED2; // turn LED2 (DS2) on
} else {
pPIO->PIO_SODR = LED2; // turn LED2 (DS2) off
}
}
------------------------------------------
unsigned enableIRQ(void)
{
unsigned _cpsr;
_cpsr = __get_cpsr();
__set_cpsr(_cpsr & ~IRQ_MASK);
return _cpsr;
}