- Sun Sep 03, 2006 11:26 pm
#18309
Hi
I am hacing the same problem......but I sstill can't see whats going on! I can write to the SD Card.....but can't read it..i get the 0x00 response....here is some of my code:
/*-------------------------------------------------------------------------
SD Read Block
Reads 512 Byte Block from the SD card
Send READ_SINGLE_BLOCK command first, wait for response come back
0x00 followed by 0xFE. The call SPI_Receive() to read the data
block back followed by the checksum.
---------------------------------------------------------------------------*/
uint32_t SD_Read_Block(uint32_t block_number)
{
uint32_t Checksum;
uint32_t varh, varl;
SPI_IOSET = SPI_SS_PIN; // Set SPI SSEL
varl = ((block_number&0x003F)<<9);
varh = ((block_number&0xFFC0)>>7);
/* Send SD CMD17(READ_SINGLE_BLOCK) to read the data from the SD card. */
SDCmd[0] = 0x51; // 1010001
/* High block address bits, varh HIGH and LOW. */
SDCmd[1] = varh >> 0x08;
SDCmd[2] = varh & 0xFF;
/* low block address bits, varl HIGH and LOW. */
SDCmd[3] = varl >> 0x08;
SDCmd[4] = varl & 0xFF;
/* Checksum is no longer required but we always send 0xFF. */
SDCmd[5] = 0xFF;
SPI_Send(SDCmd, SD_CMD_SIZE);
/* If sd_response returns 1 when we failed to get a 0x00 response. */
if ((SD_Response(0x00)) == 1);
{
SDStatus = READ_BLOCK_TIMEOUT;
SPI_IOSET = SPI_SS_PIN; // Set SPI SSEL
return SDStatus;
}
/* Wait for data token. */
if ((SD_Response(0xFE)) == 1)
{
SDStatus = READ_BLOCK_DATA_TOKEN_MISSING;
SPI_IOSET = SPI_SS_PIN; // Set SPI SSEL
return SDStatus;
}
/* Get the block of data based on the length. */
SPI_Receive(SDRDData, SD_DATA_SIZE);
/* CRC bytes that are not needed. */
Checksum = SPI_ReceiveByte();
Checksum = Checksum << 0x08 | SPI_ReceiveByte();
SPI_IOSET = SPI_SS_PIN; // Set SPI SSEL
SPI_ReceiveByte();
return 0;
}
/*-----------------------------------------------------------
SD Get Response
Repeatedly reads the SD card until we get the response we want
or timeout.
-------------------------------------------------------------*/
uint32_t SD_Response(uint8_t response)
{
uint32_t count = 0xFFF;
while( (SPI_ReceiveByte() != response) && count)
{
count--;
}
if (count == 0)
return 1; // Failure, loop was exited due to timeout
else
return 0; // Normal, loop was exited before timeout
}
any ideas?